Part Number: CDCLVD1204 How should unused inputs be connected?
The current data sheet says it is ok to leave them floating in section 8.4 but then figure 15 recommends for the unused inputs to be tied to ground via 1k ohm resistors.
Part Number: CDCLVD1204 Other Parts Discussed in Thread: CDCLVD1213 Section 11.3 describes a current draw of 186mA and a supply voltage of 3.6V, 669.6mW
The part is rated 2.5V so this does not look like a correct example. The guidance provided indicates…
Part Number: CDCLVD1204 Other Parts Discussed in Thread: LMK00338 , LMK00334 Hi Guys
Our customer is designing new generation server product. But there some questions about the PCIe Gen4 clock selection:
1. Can the previous PCIe Gen3 clk buffer product…
Part Number: CDCLVD1204 Hi,
Could you let me know the mean of "Differential input voltage peak-to-peak" in datasheet, plaese?
I understand this spec as below. is it correct?
Best regards, Shimizu
Part Number: CDCLVD1204 Other Parts Discussed in Thread: LMX2531 Dear Team,
Can we use the CDCLVD1204 with sinewave input from one of our LMX devices (Single ended - 50ohm input) ?
How do you expect the performance to degrade in this case ?
Best regards…
Part Number: CDCLVD1204 Hello
For CDCLVD1204RGTT: Can you please advise what is the max. absolute rating for the junction temp? Do you have a graph for MTBF vs. junction temp?
Thanks
Part Number: CDCLVD1208 Other Parts Discussed in Thread: CDCLVD1204 Hello,
I'm looking for additive phase noise data similar to that shown on page 6 of the CDCLVD1208 datasheet:
Specifically, I need the phase noise data for the following clock…
Part Number: CDCLVD1204 Hi,
The output connection point of the CDCLVD1204 is the FPGA of the HSTL input. In the connection configuration, LVDS ⇒ CDCLVD1204 ⇒ FPGA(HSTL)
Please tell me how to connect CDCLVD1204(out) and HSTL(input) (termination…
Part Number: CDCLVD1204 Hi,
I have a OCXO 3.3V single ended input to the CDCLVD1204.
What is the best way to interface to the input of the CDCLVD1204?
Something like this:
Were Rs is something like 50 Ohms, to reduce the voltage swing to 1.6Vpp?
…