Part Number: CDCLVD1208 Hi, Is ICCSTAT included in ICC100 and ICC800? I want to know the maximum current consumption of this device. Could you tell me how to calculate the maximum current consumption. Best Regards, Yusuke
Part Number: CDCLVD1208 Other Parts Discussed in Thread: LMK04808 The input specs of the buffer show a differential input range of 0.3V – 1.6V. But the output specs of the buffer show the differential output magnitude to be from 250mV to 450mV. Does this…
Part Number: CDCLVD1208 Other Parts Discussed in Thread: CDCLVD1204 Hello,
I'm looking for additive phase noise data similar to that shown on page 6 of the CDCLVD1208 datasheet:
Specifically, I need the phase noise data for the following clock…
Other Parts Discussed in Thread: CDCLVD1208 Hi folks -
Can I use the CDCLVD1208 to drive an 80 ohm differential pair instead of 100 ohms? Assume a 40 ohm to VTT termination on each end.
Will the IBIS model be valid for this case?
Thanks much,
Jake
Part Number: CDCLVD1208 Hello Team,
I have a customer who is using the CDCLVD1208 in their design and has reached out with the following question :
For example, if the connection of positive signal of the differential pair (CLK_100_T/F) is somehow broken…
Other Parts Discussed in Thread: CDCLVD1216 , CDCLVD1212 , CDCLVD1208 Can you clarify something in the data sheets for CDCLVD1208, CDCLVD1212, CDCLVD1216 for me?
The data sheet specs for part to part skew, propagation delay typ and max do not seem to be…
Other Parts Discussed in Thread: CDCLVD1208 Hi,
I am using 100 MHz AC coupled input for CDCLVD1208. I use 100 ohm parallel termination between differential clock lines and capacitors in series. What happens if i dint use VAC-REF pins.
Thanks in advan…
Alfred Key said:
The factory recommends to pull the unused differential input of the CDCLVD1208 to a status level by having a pull-dn on the P-input and a pull-up on the N-input.
Matt Sunna said:
The CDCLVD12xx input buffers do have hysterisis built…