Part Number: CDCLVP1102 Dear Sir/Madam,
in our project we used CDCLVP1102 as input trigger interface to the FPGA. As the chip is LVPCEL it is powered with 3.3V and the FPGA bank is powered with 1.8v. According the FPGA documents , the LVDS IVDiff is…
Part Number: CDCLVP1102 Tool/software: Hi, I am planning to use CDCLVP1102 in my design. Datasheet shows it works at 2GHz. Our designed frequency is 122.8MHz. Will it work at this frequency.
Thanks,
Syed
Part Number: CDCLVP1102 Dear TI Engineer,
We are using the CDCLVP1102 to convert a 3.3 V, 10 MHz clock signal into an LVPECL signal, which is then fed into a clock device.
In the application report SCAA056 , the calculation methods for the termination…
Part Number: CDCLVP1102 Tool/software: Hi
According to the datasheet, the orientation of the MPN CDCLVP1102RGTR indicates that pin 1 is located at Q2. However, we require pin 1 to be positioned at Q1. Could you please confirm if this option is avai…
Part Number: CDCLVP1102 Tool/software: Hello team,
My customer would like input AC-coupled single-end clock to this device. (They can't use DC coupled)
How should I configure the input to CDCLVP1102?
I am thinking as figure below. Could you please…
Part Number: CDCLVP1102 Other Parts Discussed in Thread: LMK1D1208 Tool/software:
The CDCLVP1102 datasheet lists maximum Differential input peak-peak voltage as 1.5V. Figure 14 shows a DC-coupled LVCMOS as an input to INP, with INN biased to 1/2 of…
Part Number: CDCLVP1102 Hi Teams,
Happy new year for 2024!
My customer is considering CDCLVP1102 and has some questions need to answer:
1. Can you provide the recommended application schematic diagram?
2.Customers need two outputs to reach the…
Part Number: CDCLVP1102 Tool/software: Hi,
Does the CDCLVP1102 require any duty cycle for the input? Can it be used for example for PPS (Pulse Per Second) applications where the duty cycle might typically be like 0.002%.
Thanks,
Part Number: CDCLVP1102 Hi,
The c_comp of the differential input of the IBIS model is 0.3pF, but the Icap input in the datesheet is 5pF, Δv/ΔT=1.5v/ns, both of which describe the input capacitance of the transistor. Why is there such a big difference…
Part Number: CDCLVP1102 Tool/software: Hi,
Does anyone have the temperature coefficient of propagation delay for this differential PECL input dual differential PECL output part?
Nathan