Part Number: CDCLVP111-SP Hello,
Is a pulldown resistor required to pull the CLK_SEL pin to GND? If so, what is an appropriate value? I didn't see any mention of a pulldown in the eval board design and the datasheet, but just wanted to make sure.
…
Part Number: CDCLVP111-SP The maximum operating junction temperature listed in table 5.1 for CDCLVP111-SP is +150C. The DLA spec, 5962-16207, lists the maximum operating junction temperature as +125C. Is there an error in one of these documents or do…
Part Number: CDCLVP111 Tool/software: Hello,
I'm using the rev B IBIS model to check my 2.5GHz and 200MHz clock quality. I have put 86ohm of termination to ground following the datasheet. My questions are:
1. Is CDCLVP111 output a pull up open drain…
Part Number: CDCLVP111-EP Hi Team,
Posting on behalf of our customer.
I am involved in radiation tolerance testing. Can you tell me please if any sort of DC or AC biasing is necessary on the CDCLVP111-EP to check the AC electrical characteristics…
Part Number: CDCLVP111-EP Hi,
I am not using all of the part outputs. Since there is no way to disable those outputs, what termination should I add to avoide EM noise?
Thanks
Noam
Part Number: CDCLVP111-SP Hi, we're exceeding our temp limit for this part. We only use 6 of the 10 outputs. Can I assume power is 6/10ths of the total 405mA worst case. Or do you have a better method for the caclulation?
Thanks,
Part Number: CDCLVP111-SEP Other Parts Discussed in Thread: CDCLVP111-SP The typical additive jitter foir the CDCLVP111-SEP is 0.125ps.
The max additive jitter is 0.8ps
What factors are responsible for the 0.8ps jitter performance, which is well beyond…
Part Number: CDCLVP111-SEP The typical additive jitter foir the CDCLVP111-SEP is 0.125ps.
The max additive jitter is 0.8ps
What factors are responsible for the 0.8ps jitter performance, which is well beyond what we are measuring in the lab?
What…