Part Number: CDCLVP1204 Hi Team,
Customer is consulting how to measure below input edge input? Should they measure the single-end input signal or differential input signal? Thanks
Best,
Stanley
Part Number: CDCLVP1204 Other Parts Discussed in Thread: LMK61E2 , , TLK10031
I am connecting CDCLP1204 with LMK61E2 as per the below image.
Please verify the above schematics & provide any extra terminations to be provided?
Part Number: CDCLVP1204 Hi team,
My customer wants to use the CDCLVP1204 in the system, but we have two concerns below want to double check with you.
1. As you know our device output peak to peak is 0.6V~1.35V, but the customer's requirement is 0.8V…
Part Number: CDCLVP1204 Hi Team,
This is Brandon. we met an problem on CDCLVP1204. i attached the schemtic below:
since our datasheet only refer the DC coupling,we would like to check the how should we adjust the input and output for AC coupling?
for now…
Part Number: ADC3421 Other Parts Discussed in Thread: CDCLVP2102 , LMK00304 , CDCLVP1204 Tool/software: Hi all
My customer plans to be using 3 x ADC3421IRTQR and they have this question:
Is it ok to drive the 3 ADCs with the same clock ?
(Pin 21 und Pin…
Part Number: CDCLVP1204 Hello,
We're observing some odd behaviour with the CDCLVP1204 during input switch over. Our system is as follows:
Both inputs are 156.25MHz
Both inputs are AC coupled (with 100nF caps) LVPECL signals and terminated with…
Part Number: CDCLVP1204 Hi team,
My customer is using the device CDCLVP1204RGTR now as a PCIE 100M clock buffer. For the buffer output connect to a connector, may have hotswap condition.
We want to check whether the device can support the hotswap situation. If yes…
Part Number: CDCLVP1204 Hi team,
My customer is planning to use a 200MHz LVPECL clock. For the configuration below, they want to drive the CDCLVP1204 single-ended with a square-wave. What is the recommended minimum voltage? I see recommended specs for…
Part Number: CDCLVP1204 Hi team,
My customer is using the CDCLVP1204 now. The input is LVPECL, but the input Vpp is above the datasheet spec. Do we have some methods to reduce the it?
if we change another LVPECL, the clk has a drop down curve. Do we have som…