Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed from November 25 through December 2. Thank you for your patience.
Hi Ella,
Thanks for your patience!
CDCM7005 LVPECL VOD can be higher up to 900mV at lower frequencies over the PVT. The variation can be +/-30mV over the VOD plot on Figure - 5.
Thanks!
Regards,
Ajeet Pal
Part Number: CDCM7005-SP Hello,
We are able to turn the power to our VCXO off and on, and I have recently noticed that the STATUS_VCXO pin will change to high with no input. I have put a scope on the VCXO output and there is nothing there, but the STATUS_VCXO…
Part Number: CDCM7005-SP Hello Team,
My customer has 3 questions regarding part number 5962-0723001VXC with the goal of determining max component height and making sure this part number can be used in their module design.
Regards,
Renan
Part Number: CDCM7005 Other Parts Discussed in Thread: CDCLVP111 , ,
Hi I understand that CDCLVP111 is best solution for the following usage. But, I would like you to confirm about following question.
Q. When user do not use PRI_REF and SEC_REF and use only…
Part Number: CDCM7005-SP Dear All
For an Space application, we would like to know how the CDCM7005-SP reacts against a jitter. Have you analized if this device is Single Event Transients sensitive? Any data? Any justification?
Regards
Part Number: CDCM7005-SP
Hi Team,
Good day! Could you help us answer the question from our customer. This might be confidential so I asked here internally.
Here it is:
1. Do performe TID on the packaged product as is? Or do you remove the lid and perform…
Part Number: CDCM7005-SP
Hello,
I see that the PRI_REF is an LVCMOS input and that the LVCMOS specifications show a Vik LVCMOS Input Clamp Voltage of -1.2V. Does this mean that the LVCMOS inputs can tolerate transients that are up to 1.2V higher than…
Part Number: CDCM7005 Other Parts Discussed in Thread: LMK00306 , LMK04906 , LMK04610 We are using the CDCM7005 to generate multiple outputs, We are connecting 110 Mhz crystal oscillator with LVPECL output biased to required voltage level. output to derive…