Part Number: CDCM9102 Hi all, My customer plans to use CDCM9102 and plans to connect the LVPECL output to the processor's CLKIN with AC coupling. CDCM9102 |VOD| of LVPECL is between 0.6V and 1.23V. However the VOD of CLKIN specification of processor…
Part Number: CDCM9102
We are using the clock generator part number CDCM9102. With this we are not getting the crystal clock. Whenever we keep the probe, then clock is coming for some time after that DC is coming 1.8V. We tested with two different crystal…
Hi N.V.Subbaiah,
Thank you for your effort to debug it. Earlier 1.3V on RSTOUT pin would make an unsuccessful reset in chip internal at the beginning, and is hard to return to normal status with reset again.
CDCM9102 datasheet provides 2 methods to…
Other Parts Discussed in Thread: CDCM9102 Hi all. My customer uses CDCM9102 by HCSL output. My customer would like to know 100MHz output accuracy(±~ppm or ±~MHz). Please tell me the value. Best Regards, Sho
Hi Furkan,
Just wanted to confirm with you that you are aware the CDCM9102 is a fixed 100MHz output and will not sample this device at 800MSPS. The CDCE62005 is a bit more complex. I suggest you look at and use our clocking products software ( https:/…
Other Parts Discussed in Thread: CDCM9102 Hello,
I am having an issue selecting the crystal for the CDCM9102 clock generator. We are using the CDCM9102 for a PCIe clock generator for the AM572x processor.
All the crystals suggested in the CDCM9102 datasheet…
Other Parts Discussed in Thread: CDCM9102 Can you please point me to the best app note or source of information in order to better understand the I/O structure of the clock drivers on the CDCM9102? I would very much like to see block diagrams & descriptions…
Other Parts Discussed in Thread: CDCM9102 , CDCM6100XEVM Hello,
My customer has a question about CDCM9102.
[Background]
They generated a delay by applying a 47nF capacitor to gnd on the RESET pin.
They don't use the recommended crystal.(datasheet P.11 Table…
Hi TI Experts,
Please let me confirm the following question.
[Question]
AM572x EVM used the CDCM9102RHBR for PCIe as LVDS clock. If change the clock type from LVDS to HSCL, how should we change the termination circuit?
If you have any question, please…