Part Number: CDCS503-Q1 Other Parts Discussed in Thread: CDCE913-Q1 , CDCE6214-Q1 , CDCE913 , CDCE6214 , CDCEL913 Hi Sirs, Would you please provide a recommended part similar to CDCS503-Q1 but support 100MHz, 150MHz, 200MHz with +/-2% spread spectrum…
Part Number: CDCS503 Hi team,
My customer is considering to use the CDCS503. Could you support the questions below?
1. Is it okay if the SSCG input clock stops then returns?
2. Is it necessary to have a Delay time for the output to be valid after…
Part Number: CDCS503 Hello experts,
My customer is looking for the device which meets the requirement as below;
Input : LVCMOS 3.3V (4~12MHz)
Output : LVCMOS 3.3V, single channel
Multiplication : x2 ~ x4 (From 4~12MHz clock, they want to make…
Part Number: CDCS503 Other Parts Discussed in Thread: CDCS502PERF-EVM , CDCI6214 Hi,
is there a part similar to CDCS503 that can do 5% SSC?
Thank you!
Best regards,
Alberto
Part Number: CDCS503 Other Parts Discussed in Thread: CDCE913 , , CDCS501 SSC used at Sensor Clock 37.125MHz,
Input 37.125MHz, Output 37.125MHz + 1% SSC
1.
can you help to recommend suitable Spread-Spectrum Clocking recommend?
501 and 503 freq…
Other Parts Discussed in Thread: CDCS503 , CDCVF2505 , CDCV304 , CDCLVC1102 Hi,
we want to use CDCS503 for 9.4Mhz buffer, request input and output same phase, we test CDCS503, output phase cannot control? setting:OE high, FS SSC_SEL0,SSC_SEL 1 low.…
Other Parts Discussed in Thread: CDCS503 , LMV7219 , LMH7220 , LMH7322 , LMH7324 , DS90UR124 , DS90UR241 Customer video process output clk is a triangle wave, we want reshape that to square wave, Does CDCS503 can do that or suggest other part(frequency…
Part Number: CDCS504-Q1 Other Parts Discussed in Thread: CDCS503 , LMK1C1104 Tool/software: Hi, Team
Customer just check with TI, whether we have non-Q device for CDCS504-Q1? Or which device have similar function with CDCS504-Q1 with non-Q?
customer…
Sienna,
Does the device that they need require the extended temperature rating, and do they have a crystal or LVCMOS clock input? If LVCMOS, the CDCS503-Q1 ( https://www.ti.com/lit/ds/symlink/cdcs503-q1.pdf ) is a suitable solution.
Thanks,
Kad…