This is the first answer of googling "eagle nexfet footprint". Seen to be nobody has posted yet, here is a library with NexFET Block SON-5X6 and 3x3. modify according to your needs.
5025.nexfet.zip
Other Parts Discussed in Thread: CSD16301Q2 Hi,
On the data sheet of CSD16301Q2, The Rds(on) resistance is shown as 27mohms (TYP) at Vgs=3V, Ids=4A conduction.
I am wondering that if Ids is 0.5A (or even smaller, like 0.1A) what is the Rds(on) resistance…
Part Number: CSD16327Q3 Other Parts Discussed in Thread: TINA-TI , CSD13303W1015 , CSD16301Q2 Tool/software: Hello,
I downloaded this PSpice model file and inserted into cadence PSPICE file tab and click. The simulation can run through(without generate…
Part Number: TPS552882 Other Parts Discussed in Thread: CSD15571Q2 , CSD16301Q2 Hi,
We're building an LED matrix display, and are using two independant TPS552882 power supplies. The design criteria for these two supplies is as follows:
White LED…
Hi Friedl,
Thanks for reaching out!
TPS2663 can drive CSD16301Q2 FET but there would be slightly higher turn-on delay with CSD16301Q2 over BSS138 due to higher Ciss capacitance however the low Ron of CSD16301Q2 greatly reduces the t(Driver) time to…
Part Number: SN74LVC1G07 Other Parts Discussed in Thread: CSD16301Q2 , SN74LVC1T45 Hi team,
My customer is using SN74LVC1G07 for level shifter and external pull to drive an MOSFET CSD16301Q2. Does this circuit have any problem or not? Customer input…
Part Number: TPS55288-Q1 Other Parts Discussed in Thread: CSD16301Q2 , TPS55288 , TPS552882 Hello! I am working on my own power bank application and to charge my battery (which for the purposes of assemblying was NOT connected during my tests so far)…
Part Number: TPS81256 Other Parts Discussed in Thread: CSD16301Q2 Hello,
I'm using the TPS81256 to supply power to a laser diode module. I'm modulating the laser by using a CSD16301Q2 MOSFET on the low side of the module to modulate the connection to…
Part Number: BQ2970 Hi everyone,
I have included the BQ29707 into my design and in general it works as expected. When the battery voltage goes below 2.8V the DOUT goes LOW to interrupt the circuit ( turn OFF DSG FET ) and protect the battery from further…