Part Number: CSD17571Q2 Hello,
I am concerned about the increase in temperature of a MOSFET.
Example:
Temperature = 25 grad
I drive a power resistor, with a single pulse with ton=300ms; the current is 7A.
From the datasheet I extract Zth=0,2…
Part Number: CSD17571Q2 Hi team,
It is nice to know you here. I want to penetrate CSD17571Q2 to my customer to do Active Mille CLAMP function, the circuit should be like below. The Vs may some 200ns pulse and the peak voltage should lower than 2V or…
Hi Roger,
Thanks for the questions. If you're using a N-channel FET such as CSD17571Q2 as a high side load switch, you will need to drive the gate to at least 4.5V greater than the input voltage. Since 19V is the highest available voltage on the board…
Part Number: BQ25616 Other Parts Discussed in Thread: CSD17571Q2 Dear Technical Service,
I am trying to design a PCB with your IC BQ25616, and I am taking the section "10.2.2 BQ25616/616J Application with External OVP" as a reference. My question here…
Part Number: BQ29209 Other Parts Discussed in Thread: BQ25798 , CSD17571Q2 Tool/software: I have a design with BQ25798 BQ25798bb RQMR and BQ29209DRBR, for a 2s battery pack.
I want to use 2 CSD17571Q2 mosfets, for overvoltage protection.
I this implementation…
Part Number: TCA6408A Other Parts Discussed in Thread: CSD17571Q2 , UCC27517 Tool/software: Maybe it's just late and I'm tired, but I just want to check myself here. Can you use the I/O pins of the TC6408A to directly drive MOSFETs (specifically the CSD17571Q2…
Part Number: CSD18511KCS Other Parts Discussed in Thread: CSD17571Q2 Hi TIer
Customer needs a power MOS, 30V VDS, hope its CISS can be less than 1500pF, since TI.com does not have a direct filter to use,
Could you recommend an NMOS and PMOS to me…
Part Number: CD4050B Other Parts Discussed in Thread: CSD17571Q2 Tool/software: Hello
I wish to translate +15 V signals to 3.3V to my DSP.
Can I use CD4050B for this purpose, where the Vdd is 3.3V
( A similar IC from Onsemi MC14050 specifies a Vdd…
Part Number: LM5050-1-Q1 Other Parts Discussed in Thread: LM74700-Q1 , , CSD17571Q2 , LM5050-1 ALL HI!
What is the difference between lm5050 and lm74700-q1 in use function? Whether it can be used interchangeably. My use requirements are: 1. Prevent…
Part Number: CSD19538Q2 Other Parts Discussed in Thread: CSD16301Q2 , CSD17571Q2 , Hi,
My customer need below auto grade MOS. please kindly recommend accordingly. thanks.
CSD16301Q2_25V_5A_TI
CSD17571Q2_30V_22A_TI
CSD19538Q2_100V_14…