Part Number: DAC80501 Other Parts Discussed in Thread: DAC11001A Hi Experts, Good day. Our customer is asking how to calculate the accuracy of DAC80501. please advise. Keep safe. Regards,
Josel
Other Parts Discussed in Thread: DAC11001A , PGA202 , PGA103 , PGA280 , PGA281 , OPA4182 , OPA4191 , OPA1604 I am looking for a PGA for the output from DAC11001A to be able to output up to +/-10V, but also take a 5V output down to 0.5V. Do you have any…
Part Number: DAC1220 Other Parts Discussed in Thread: DAC8560 , DAC11001A Hi Team,
Hope everything goes well. One customer were facing a problem while using our DAC1220.
Q: when system power up, it will takes 100ms for MCU(F2803x) to wake up. Before…
Hi Christian,
I think you should look at our new 20-bit flagship precision DAC, the DAC11001A. This device is an R-2R device, so it will have excellent DC specs. In addition, it has a very capable track-and-hold subcircuit that keeps code-to-code glitch…
Hi,
Are you looking for specifically over 2.2MHz update rate? if that's the case , we don't have any device from our precision DAC portfolio.
However our high speed DAC family has vast selection of DAC's which will satisfy all the conditions you mentioned…
Part Number: DAC8831EVM Other Parts Discussed in Thread: DAC8871EVM , , DAC8831 , DAC8871 , DAC11001A Hello Team,
It is possible to control the output of the DAC8831EVM, DAC8871EVM and DAC11001A-EVM per normal SPI code from a Arduino library? I mean…
Hi,
What kind of resolution are you looking at? For this 10KHz sine wave generation, please have a look at the below options.
R2R Unbuffered 16,18,20bits DAC
DAC11001A data sheet, product information and support | TI.com
MDAC's
DAC8811 data…
Hi,
Can you please look at DAC11001.
This device should be able to do the arbitrary waveform generation with the mentioned frequency range.
DAC11001A data sheet, product information and support | TI.com
BP-DAC11001EVM Evaluation board | TI.com…
Part Number: PCM5102A Other Parts Discussed in Thread: DAC80502 , DAC11001A Hi Sirs,
Did PCM5102A support to output 3~20Hz audio signal or not?
If yes, what the performance it is?
Thanks.