Other Parts Discussed in Thread: DAC128S085 I am in the process of designing board hardware using the DAC128S085 (12-bit DAC) and need some clarification regarding the voltage range for VREF1 and VREF2 in the datasheet.
On page 1, section 3 (description…
Part Number: TLV9304 Other Parts Discussed in Thread: DAC128S085 , TLV9302 , , TLV4172 , OPA4191 Hai Sir,
My End application is - Controlling & Analog outputs driving.
We are planning to generate the 0-10V & ±10V output using Opamp-TLV9304.…
Part Number: TMS320F280025C Other Parts Discussed in Thread: SFRA , DRV8329AEVM , DAC128S085 hi team
i have faced Compilation failure error, kindly check let me know the your feedback.
>> Compilation failure src_board/subdir_rules.mk:9: recipe for target…
Forgot to include them, here's the compiler options: The version is v22.6.0.LTS
**** Build of configuration Flash_lib_DRV8323RH_3SC for project universal_motorcontrol_lab_f28003x ****
"C:\\ti\\ccs1240\\ccs\\utils\\bin\\gmake" -k -j 12 src_control…
Part Number: DRV8343S-Q1EVM Other Parts Discussed in Thread: SFRA , C2000WARE , DAC128S085 Dear team
we are working Launchpad f280025c - 80 pin with drv8343 interfaced both EVM , sensroless bldc motor connected under universal motor control reused adc and pwm…
Other Parts Discussed in Thread: DAC128S085 Hi-
For DAC128S085, can the Reference input(s) to the part be applied when the Power supply to the part is 0V?
If so, will we get excessive current due to protection diodes?
Thanks,
-Tim Starr on behalf of RW…
Hi,
I don't think any issue with Win10 as we have other users who evaluated with Win 10 machine and it works.
e2e.ti.com/.../dac128s085evm-replace-from-dac128s085-to-dac108s085
I will order an EVM to test this. Please hold on.
Regards,
AK
Hi Faisal,
From a hardware standpoint the DAC128S085EVM would directly connect to the LAUNCHXL-F28379D board's boosterpack connectors and the SPI connections will be properly made. The more difficult part is creating a SPI software driver to interface…
Yes. I ran the other motor and id did just fine,
Yes I ran it after my software changes,
yes I ran it after I have changed the voltage and current range changes,
yes I changed the scale settings in user.h according to the changed voltage and current ranges…