Hi Danny,
Regarding the pins which are labeled as NC, I suggest to leave these floating. Whenever you come across a discrepancy between schematic symbol and the datasheet, it is always recommended to use the information provided in the datasheet as it…
Part Number: DAC3154 Other Parts Discussed in Thread: DAC3152 , I'm comparing both DACs (DAC3152) & (DAC3154) and I'm trying to find, which one is more suitable for my design.
In datasheet for DAC3152 it's mentioned, that the preferred input…
Part Number: DAC3154 I am trying to write both default and non-default values to some registers (specifically 0x44E4 to config0 or some clkdelay values to config3).
It seems that any write to these registers halts operation of the DAC (as viewed from…
Part Number: DAC3154 Hello,
I will be driving the DAC3154 from a Xilinx Series 7 FPGA (using the OSERDESE2) and wish to use the single 10 bit bus to multiplex data for both A and B DACS on the chip.
In this situation the output SERDES from the FPGA can…
Part Number: DAC3154 I am trying to understand from the data sheet how to best drive both DACCLK and DATACLK.
DATACLK: Should I drive it LVDS AC or DC coupled? I understand that the device has internal 100ohm termination.
DACCLK: Should be driven LVPECL…
Part Number: DAC3154 Other Parts Discussed in Thread: DAC3174 Hi Team, Our customer would like to request for the junction temperature information for DAC3154 because it is not available in the datasheet. Thanks! Jonathan
Other Parts Discussed in Thread: DAC3174 , DAC3171 , DAC3484 , OPA695 , THS3215 Hello there,
From the schematics of DAC31X1 EVM and DAC3174 EVM, the outputs of DAC31X1 and DAC3174 are AC-coupled. Can you recommend implementations of DC-coupled outputs?
Many…
Part Number: THS3491 Other Parts Discussed in Thread: DAC3154 , THS3217 , Hello,
I have designed the post-DAC amplifier from good ideas mentioned on this forum.
The input to this stage is driven directly from current output DAC3154.
The board is up and running…
Part Number: DAC3174 Other Parts Discussed in Thread: DAC3164 , DAC3151 , DAC3171 , DAC3154 , , DAC3161 Hi,
In DA3174 datasheet (SLAS837B –APRIL 2013–REVISED JANUARY 2017)
Pins 63,62,52,51 are marked as NC in "Pin Functions" Table it is mentioned…
Part Number: DAC3154EVM Other Parts Discussed in Thread: DAC3154 , DAC3174 , TRF3705 Hi, I am trying to use the DAC3154 Dual-Channel, 10-Bit, 500-MSPS Digital-to-Analog Converter Evaluation Module. I connected the a 10 MHz clock to CDCE input.Using the DAC3174_v1p2…