Part Number: DAC3283 We see spurs in our RF output and we believe it is coming from the DAC. Are there any registers for this DAC that we can adjust to reduce the level of the spurs. These spurs might also be coming from the IF, but is there a way to…
Part Number: DAC3283 Hi ,
We are using DAC3283 in dual sync mode and trying to do phase matching.
Our setup includes 4 DAC3283 devices operating at 800MHz, with an IF range of 65MHz to 75MHz.
We are performing 4× interpolation within the DAC.…
Part Number: DAC3283 Tool/software: Hi Team,
My board clock requirement block diagram is attached below.
The clock from the clock synthesizer need to feed as input clock to all ADC, DAC and FPGA in the board to make a synchronization.
Also from…
Part Number: DAC3283 Dear Team,
We are currently working on a custom board design that uses an Texas Instrument DAC, and we would like your guidance on a grounding-related implementation detail to ensure compliance with best practices and datasheet…
Part Number: DAC3283 Tool/software: Hello,
we are using this DAC in our product: DAC3283
we would like to know when and how this temperature alarm is generated. as in our case it seems we get this alarm quiet often.
also is the temperature…
Part Number: DAC3283
Tool/software:
Hi
I am using DAC3283 in my application.
DATACLKx = 400 MHz
DACCLKPx = 400 MHz
OSTRx = 1.25 MHz.
FRAMEx = 3.125 MHz
Interpolation = x2
With these configurations, DAC Linkup works, and I can send correct…
Part Number: DAC3283 I’m using four DAC3283 devices, with both the clock and OSTRP signals generated by the HMC7044. I need guidance on how to interface the OSTRP signal—configured in LVPECL mode—from the HMC7044 to the DAC3283, considering that OSTRP…
Part Number: DAC3283 Other Parts Discussed in Thread: DAC5689 Tool/software: Hi Team,
I'm planning to use the DAC IC DAC3283 in my board.
I have one query regarding the IC. I want an input Frame Sync or Clock Sync signal which must be coming from…
Part Number: LMK04832 Other Parts Discussed in Thread: DAC3283 Tool/software: Hi,
I am planning to use 4 DAC3283 DACs for my Analog signal generation. I need to phase match all the 8 outputs of DAC (2 from 4 each), and planning to provide DAC Clock…
Part Number: DAC3283 Other Parts Discussed in Thread: ADS62P49 I am working on DAC3283 eval board SPI interface with zcu106 FPGA evaluation board using FMC connector. For that we have used FMC DAC adapter(from TI). But when we referred to the schematics…