Hello Mastik,
We have reviewed the amplifiers in the schematic:
THS4021
This is a decompensated amplifier with a gain requirement of 10V/V. The note says Gain of 12, but the configuration shows around 7V/V.
The DAC is current source output with 300kOhm…
Part Number: ADS42LB69 I am attaching the adc-dac schematic.
Please review and let me know if any changes are required. adc_dac.pdf
Please let me know the LVDS voltage level for clock inputs & Output.
Please let me know the value of Vcm for DAC and…
Part Number: DAC5652A Hi,
In DAC5652A datasheet and in all the corresponding links in your site, the thermal pad size is missing. It just saying " SIZE AND SHAPE SHOWN ON SEPARATE SHEET: which I couldn't find...
Can you please correct the datasheet…
David,
The only thing I can provide is that the first digit is always the year, and the second digit is always the month, and the ECAT is underlined.
Regards,
Jim
Part Number: DAC5652A Other Parts Discussed in Thread: DAC5652 Hi
We plan to use DAC5652 to design, we don't understand some parameters. We need help to confirm, thanks
1. How to understand IOUTFS = 0 dB or -6 , -12 dB about AC Linearity ?
2. What…
Part Number: DAC5652A Hello,
I'm currently working on the data timing for the DAC5652A in Dual-Bus Mode. I'm trying to give data to four different DAC5652A as fast as possible, but they share the same data lines. What is the fastest way to send…
Part Number: DAC5652A Hello,
Our customer use the DAC5652A.
The customer want to output zero temporary. (IOUTFS=0)
They are considering two ways.
First, they use an external reference and apply 0V to Vref.
Second, they disconnect the RSET .
Are these…
Part Number: DAC5652A Hello,
Our customer use the DAC5652A, have a question.
How long does it take to accept the clock signal after the SLEEP pin High to Low?
Best Regards,
Naoki Aoyama