Hi,
I am attaching simple header file for DAC80502. You can modify the same to make it work for DAC60501.
Let me know if you need more help.
Regards,
AK 8814.dac80502.h
Part Number: REF5050 Other Parts Discussed in Thread: DAC80502 Dear Technical Support Team,
REF5050 is used for DAC80502.
Expected output voltage of REF5050 is 5V, however it shows 2.5V.
Input voltage is 10V and I can see it with oscilloscope. …
Hi,
We don't have source code per say, But we do provide header files for DAC8050x devices which can be used by customers for faster development. I am attaching one for DAC80502. Just change these to get started.
dac80502.h
Regards,
AK
Hi Kevin,
You can start by looking at this header file for register definitions:
https://e2e.ti.com/support/data-converters-group/data-converters/f/data-converters-forum/966178/dac80502-faq-dac80502-faq-are-there-source-code-or-header-file-examples…
Part Number: PCM5102A Other Parts Discussed in Thread: DAC80502 , DAC11001A Hi Sirs,
Did PCM5102A support to output 3~20Hz audio signal or not?
If yes, what the performance it is?
Thanks.
Hi Holly,
We don't have any example C code for this device. However I can share header file from the same family of device. You just need to update this with correct register values.
DAC80508 has simple and standard SPI interface, let me know if you…
Other Parts Discussed in Thread: DAC80502 Hi Team, I am assisting a customer that needs some application inputs. Below is his inquiry, hoping if you can help us identify what type of application he is needing.
1) I need a part which can work with various…
Hi,
Correct me if I am wrong . If you remove 3rd harmonics completely from saw tooth, it will add distortion right? Because 3rd harmonics is the dominant factor to create a saw tooth in first place.
Anyway since your application frequency is 60Hz…
Hi,
I had checked this with our design team. There is a problem in the product datasheet. Please find the device ID's.
DAC80501Z 0x0115
DAC70501Z 0x1115
DAC60501Z 0x2115
DAC80501M 0x0195
DAC70501M 0x1195
DAC60501M 0x2195
DAC80502 0x0215…
Part Number: PCM5122 Other Parts Discussed in Thread: DAC80502 , DAC8822 , DAC11001A , PCM5100A Help me please with understand why this is so. PCM5122. I am studying the work of PCM5122. I'm using Raspberry Pi. Everything works well.
I can't figure…