Part Number: ADS1256 Other Parts Discussed in Thread: DAC8532
Hi,
when I'm using the ADS1256 in the continuous mode at 30SPS my first conversion result should appear after about 5 conversions periods.
To test that behavior I gave the ADS1256 an impulse…
Other Parts Discussed in Thread: DAC8532 , PCM5100A , DAC8811 hi all,
I need to produce a sine wave with the frequency of 1k to 100kHZ, and amplitude of 1mV~100mV, can you give a a recommendation IC for that , thanks, Can I use DAC8532 for that.
and i also…
Hello Chris,
thanks for your fast response!
I will try to use a single crystal and multiply voltage references.
I have additional questions:
Can i use a single power supply with pi filter to power all the ADCs? The reference voltage will be powered…
Part Number: ADS1256 Other Parts Discussed in Thread: DAC8532 Hi,
I bought a high-precision AD/DA board form Waveshare that uses the ADS1256 as ADC. They provide an example program to read the analog values but this goes rather slow.
Can someone help…
Other Parts Discussed in Thread: LAUNCHXL-F28379D , DAC8532 I need a DSP Board that has 16 bit analog in and 16 bit analog out. Most boards seem to be 12 bit devices. I was thinking of trying to use a LAUNCHXL-F28379D but I can't find a boosterpack that…
In the normal system on state the switches are set to allow the DAC8532 to operate the VCA. I have an opamp circuit to invert and attenuate the DAC voltage. The DAC is set to active but should be set to 0V level up at system start so I would say no. The…