Hi Javier,
I don't think this will work with newer high resolution Multiplying DACs.I do know that 16-bit devices have reduced linearity when used in this configuration. I need to gather more information from our designer to see of I can give you…
Other Parts Discussed in Thread: DAC8801 I am trying to characterize some power up/down behavior we are experiencing with in an application using the DAC8801. Upon a power cycle, approximately 1-2 sec powered down, sometimes the DAC retains it's last…
Part Number: DAC7811 Other Parts Discussed in Thread: DAC8811 , DAC8801 Tool/software: Hi,
Customer want to replace AD5446.
Do we have suitable devices to replace AD5446?
DAC7811 is 12Bit, do we have 14 Bit devices?
Thank you
Yishan Chen
Part Number: DAC8411 Other Parts Discussed in Thread: DAC8801 , I was testing a DAC8801 using the DAC8801 Eval board. The SPI signals are coming from ports on an STM32F407 and are all about 3.3V signals. The DAC8801 worked very well, but we decided we…
Part Number: DAC8811EVM-PDK Other Parts Discussed in Thread: DXP , DAC8801 , DAC8811EVM Hi team, The /CS pin of J2 is always low output. Instead, I'll see the FSX pin output like output the /CE pin. Is it a configuration issue? Sincerely. Kengo.
Hi Kevin,
I'm looking at unbuffered DACs per your advice. DAC8801 current output looked good at first glance, but then it looks like the full-scale accuracy is only 20%. Strange that its specified 20% only on the first page though, nothing about it…
Hi Cindy,
section 8.3.1 of datasheet of DAC8801 recommends the add of a compensation capacitor (C1). This cap would provide a phase lead compensation and by this decrease the ringing.
Decreasing R8 to 47R and leaving C3 at 470pF can additionally…
Hello Rajesh,
There are a few different approaches you can take here.
First is a dc REF, as described in this App Note: www.ti.com/.../litabsmultiplefilelist.tsp .
Next is a currentDAC, such as: www.ti.com/.../dac8801 .
And third, since you are…
Hi Rick,
I know this thread has grown a bit stale, but I just found it searching and wanted to chime in my interest as well.
Right now we're working on a new design, part of which uses R-2R MDACs (the DAC8801 / DAC8803 specifically) in a digitally…