Part Number: LAUNCHXL-CC1310 Other Parts Discussed in Thread: CC1310 Tool/software: I'm using the stock sensor_CC1310_LAUNCHXL_tirtos_ccs example project. In order to see how often messages were being sent out over RF, I thought I'd add a timestamp…
Part Number: TPSM828302 Other Parts Discussed in Thread: TPSM828301 Tool/software: I am thinking of using this device to drive a load less than 1A. I know that the 1A-version TPSM828301 could be used, but I want to use TPSM828302 instead in my design…
Hi Ehtan, I tried this method and I'm able to reach 50.36V on batteries. Also, charge terminates when charging current is around 100 mA (as we have set a CC current of 1A). Also, charge is re-launched when expected. So this issue is solved on this PCB…
Part Number: AM6442 Other Parts Discussed in Thread: SYSCONFIG
Tool/software:
Hello,
I have some issue with lwip running on the R5 core 0-0 of an AM64. This is the story so far :
I was able to compile lwip and use it in my project
I'm able to ping the…
sorry for late reply. i was busy with other things in testing. Since i have 9V, 1A power supply so I guess even if short circuit happens, current cant exceed 1A. but I did observe voltage behaviour.
10.27V Vin, 10.27 Vout when no short circuit. 9.73V…
Part Number: TDA4VH-Q1 Tool/software: Hi,
SDK:8.6
At present, our project needs to implement flash write protection function, and the implementation method is as follows:
When the system is powered on,configure flash write protection for the entire flash…
Part Number: TMS320F28379D Other Parts Discussed in Thread: TIDA-01606 Tool/software: Hi,
Is there a way to generate complementary signals between ePWM1, 2 and so on; a complementary signal between ePWM1A and ePWM2A ?
Generating complementary signals…
Hi,
LM5025 integrated driver with driving peak current 2A so it looks ok for 200W driving: But UCC28C43 or C53 driving with peak 1A so you need to add external driver to get 2A for 200W.
Hi Drew,
1. OK, we understood that "raw data" setting is normally recommended, but inour system, something abnormal happenned.
In our system, when CDR is unlocked,
in "raw data" setting, the signal is worse than when DS100DF410 is not implemented…
Hi Paul,
1. Correct, they are p2p compatible apart from input voltage rating.
2. Better to just use one good FET instead of two paralleled FETs, as it keeps the switching loop area to a minimum. See app note SNVA803 for more detail here. If paralleled…