Desktop linux SDK package tested in Ubuntu 12.04 LTS (3.2.0-25 kernel version).
Have you using the same version on your testing?
I have tested the DSPC8681 EVM with Ubuntu 12.04 LTS (3.2.0-38 kernel version), DSP reset command working properly. I…
Part Number: PROCESSOR-SDK-AM57X Other Parts Discussed in Thread: CCSTUDIO
I had to migrate a project from CCS 11 running on Windows, to CCS 11 running on Linux.
Since this is a different architecture, I downloaded the Linux versions of all the libraries…
Part Number: CODECOMPOSER Other Parts Discussed in Thread: PGA970 , USB2ANY Tool/software: I'm using CCS 12.8 to align with the answer given in a previous question PGA970: Programming a binary over SPI but am open to changing versions.
I am on Windows…
Hi Sreenivasa,
Thank you for your reply.
Here are the first page of Table 4-10. Pin Attributes (ZDN Package). It differs from the first pin indication in the table.
SPRS851D_am437x.pdf
SPRS851E_am437x.pdf
Best Regards, Kanae
Part Number: TUSB8041 Hi Team,
Could you help review schematic of TUSB8041 which my customer applies in their robot. Besides, I have some confusion about this device.
The schematic can be seen in this link: /cfs-file/__key/communityserver-discussions…
Part Number: TPS55288 Dear TI E2E teams,
TPS55288 is used for PD charger in my project.
it seems TPS55288 does not work fine in my test.
it can output voltage as my set, but the output power can not meet the design requirements, it just can output…
4278.am437x_mcasp.txt
Hi Pavel,
Thank you for your patience.
SDK may be ti-processor-sdk-linux-am437x-evm-03.01.00.06-Linux-x86-Install.bin,The attachment is boot log,AM437x MCASP0_AXR0 waveform of the H23 pin is as follows:
Part Number: IWR6843 I am trying to flash an IWR6843 over SPI.
At boot I get the AWR_DEV_ASYNC_EVENT_MSG with "power up done" as expected. I then send AWR_DEV_FILE_DOWNLOAD_MSG with 250 bytes of payload and I get an error without payload.
What is…
Hi, all
I'm using the DM6446 EVM. I've successfully realized the function of universal_copy by utilizing memcpy(), and now I want to accomplished it with DMAN3. By referencing the code downloaded from
http://processors.wiki.ti.com/index.php/C64x…
Part Number: TPS23880 Dear Team,
The customer uses our EVM TPS23880 4-pair to test Sifos, some of the test items fail.
Do you have any ideas why?
TI_port 5_psa_report.xls
TI_port 6_psa_report.xls
BR
Kevin