Part Number: DEM-OPA-WSON8-EVM Good afternoon, is it possible for you to provide the gerber files of the mentioned evaluation board?
Thanks in advance,
Pablo.
Part Number: DEM-OPA-WSON8-EVM Other Parts Discussed in Thread: OPA858DSGEVM , OPA858 Can you provide the size/type of passives and SMA connector for the EVM?
Regards, Bernd
Hello Lance,
We do offer the DEM-OPA-RGV-EVM , which is an generic EVM board designed for VQFN (RGV) package PLC and DSL line drivers. The associated user's guide showcases the EVM functionality, which can do either two amplifier channels or a single differential…
Joaquin,
There is an EVM available which you can get from TI.com to test yor circuit (link below)
https://www.ti.com/tool/DEM-OPA-RGV-EVM
In your schematic (snippet below) the input swings from 0V to 3.3V, so for the time period in which it is 0V, it…
Hello Prathmesh,
The closest alternative to REG104FA-5/500G3 is TL1963AKTTR, which is offered in TO-263 (KTT) package.
For REG103GA-3.3, the best alternative is TPS7A2633DRVR which is not on the same package, but similar specs. Another option is TLV76133DCYR…
Hello D,
1) I found in DS of OPA360 page6 ( Enable/Shutdown) section
"If the Enable pin is not connected, internal pull-up circuitry will enable the amplifier."
But it is probably better to tie it to 3.3V
- I agree, you may float it but I recommend…
Hi Sankalp,
I would recommend 2 pcs TPS62932 to get Input Vin 15V, output 3.3V(1A) and 5V(0.5A). It is 3.8-30V input, 2-A, 200kHz to 2.2MHz, low-IQ synchronous buck converter in SOT-583 package.
Thanks and kindly let us know anything unclear.
BRs
Luci…
Hi Ranjith,
Thank you for providing that information. We have TLV75201PDSQR as an adjustable dual LDO which each rail can handle up to 1A , and each rail is independently set. This dual LDO is adjustable with high PSRR and comes in a small package:
…