Part Number: BQ76952EVM Other Parts Discussed in Thread: BQSTUDIO Hi Max :) Thank you for you reply. I understand it.
>Hi Awatch,
>I believe that the Data Graph is limited to only 6 variables, however you can take a log of all the basic parameters with…
Part Number: ADS52J90 Hello,
I am attempting to utilize the ADS52J90 in a 32-channel mode to digitize 32 distinct analog values coming from a test chip. The data received from the test chip is not continuous in nature. Whenever the data is ready, the…
Other Parts Discussed in Thread: DAC5672A Hello,
When using a DAC, if the data clock and the data on the digital interface are out of sync, we will observe an elevated noise level adjacent to the output signal.
Could you please explain why the noise in…
Part Number: BQ76952EVM Other Parts Discussed in Thread: BQSTUDIO Hi! :)
I using BQstudio with BQ76952EVM.
I have some question for Data Graph
This device has 16ch battery monitor,
but BQ studio can dispray only 6ch.
I want dispray 16ch with BQ76952EVM…
Part Number: TDA4VM Dear Expert,
I create two or more graphs in a context, how to pass data between different graphs, for example, the output of a node in one graph as the input of another graph, how to achieve this operation, or can it be achieved? …
Part Number: MSP430F4618 Other Parts Discussed in Thread: MSP-FET
Dear Embedded Community,
My application requires sending data on P3.2. This should appear on pin 69 of the CPU. It does but this is also pulled high or low from time to time. I've seen it…
Part Number: BQSTUDIO Other Parts Discussed in Thread: BQ78350 , EV2400 Using Graphing in BQStudio, the voltage and current plots intermittently drop to zero for only one scan point then return to normal expected plot. This can occur for multiple points…
Part Number: BQSTUDIO Hello E2E Experts,
Good day.
How make a Data Graph report with this software?
Additional question: Is it possible to change the second to minutes?
Regards,
CSC
Part Number: ISOW7741DFMEVM Other Parts Discussed in Thread: ISOW7741 , ISOW7721 Hello Team,
I'm evaluating ISOW7741DFMEVM for isolating UART Signals.
My Setup is as follows
CP2102 (USB/UART Converter) TX is connected to INA of the EVM
MCU RX is connected…
Part Number: AFE5832LP Other Parts Discussed in Thread: AFE5832 , Dear Sir/Madam,
According to the datasheet of AFE5832, does it mean that AFE5832LP already finishes beamforming in CW mode and I do not need to perform further beamforming on FPGA after reading…