5468.SLUA791_bq76PL455A Design Recommendations.pdf Hello Gupta,
I didn't find problem in your schematic which is almost same as 455 EVM's.
I didn't know specs of your selected NPN. Check details in the below app note.
Andy
Part Number: TDA4VM
Hi,
I want to load mcu1_0 using rproc commands at u-boot prompt.According to the FAQ- e2e.ti.com/.../3382578 ,the r5f reset vectors should be in ATCM ,not BTCM.And I configure it as R5F_TCMA in linker.cmd.But the applications…
Hi Hai,
The SN74AVCA164245 is not a buffer, it is simply a switch. What goes in on one side comes out on the other. The SN74AVCB324245 will translate from 1.8V to 3.3V and from 3.3V to 1.8V as well as other notable voltage nodes. It provides active…
Part Number: TMDX654IDKEVM phc2sys fails to synchronize between CLOCK_REALTIME and PRU ETH ptp devices in Linux RT SDK 8.0:
root@am65xx-evm:~# phc2sys -s CLOCK_REALTIME -c /dev/ptp4 -O 0 -m phc2sys[168.791]: /dev/ptp4 sys offset -585375821865600332…
Hi,
I found a CPSW issue.
I used AM335x Starter kit with SDK 03.00.00.04 and 03.01.00.06.(Prebuilt binaries)
My testing environment:
[Host PC]192.168.1.200 <---> eth1:192.168.1.1 [AM335x] eth0:192.168.18.116 <---> 192.168.18.2 [Route Gateway…
Part Number: DRA821U Dear expert,
I debug customer board run on 7.3 SDK,use sbl boot and MCU2_0 run app_remoteswitchcfg_server_strip.xer5f. When don't boot linux via delet sd card
partition file atf_optee.appimage,I can ping customer board use PC…
Other Parts Discussed in Thread: CC2650 Hello. Have tried to install CCS6.2 from zip file onto 3 different PC's in the last 24 hours. Two win7 and one win10 only commonality is the base zipfile (md5 checks out), and the network. Urgent need to flash a…
Hello Ranjith Parakkal,
Thank you very much for the reply.
Please find the kernel log and tiler map below
Starting kernel ...
[ 0.000000] Initializing cgroup subsys cpu [ 0.000000] Linux version 3.0.21-00003-OMAP-Android+ (sanjay@mistral-Veriton…