Part Number: DP83630 Hi Team,
My customer is experiencing a communication error when inserting and extracting connector hot plug between boards.
Specifically, the LED_ACT toggle continues.
When I check the FLP burst signal, I noticed that it changed…
Hi,
DP83630 will support transformerless operation. Here is an application report for that: www.ti.com/.../snla088a.pdf
I am not sure if I understand your comment about point to point model. Do you mean the PHY and RJ-45 connector are on separate…
Part Number: DP83630 Hi Team,
Although "AUTO-CROSSOVER" and "AUTO-MDIX" have similar functions, do not use AUTO-MDIX with FORCED MODE?
Why is "AUTO-CROSSOVER" available? Is there a special reason?
Best Regards,
Kenji
Part Number: DP83630 Hi team,
My customer wants to set below configuration.
・100BASE-TX and Full-Duplex fixed ・Auto-MDIX enable
I think the custome should use the Advertised Mode(AN_EN=1/AN1=1/AN=0:100BASE-TX, Full-Duplex). Because I think that…
Hi Zach,
1. In terms of what pins are used and unused, the app note may be specific to the device. To clarify for the DP83630, TX_CLK and RX_CLK are used in RMII master mode, but unused in RMII slave mode. Please review section 3.4 of the datasheet…
Part Number: DP83630 Other Parts Discussed in Thread: DP83620 , HI Team,
I am planning to use DP83620 Ethernet PHY IC for my embedded application as a replacement of AM79C874 IC. To test the functionality of DP83620 TI is providing a EVK kit. There…
Other Parts Discussed in Thread: DP83630 Tool/software: Linux Hello,
I have some questions about the Ethernet transceiver of DP83630 :
We have a board with the AM335x processor and DP83630 ethernet Transceiver and
have to do compliance and Speed…
Part Number: DP83630 Hey,
I'm working on a project using Ethernet PYH DP83630. The datasheet specifies a max crystal tolerance of +/-50ppm and max 1-year aging of +/-50ppm.
I'm wondering may I add them up and use whatever crystal has +/-100ppm total…