Hello Krishna,
If you want to use our DP83TC812 PHY then the only way to have RJ45 as an output would be putting two DP83TC812 EVM's back to back so it would look like this:
PC -> EVM #1 RJ45 -> EVM #1 Matenet connector -> EVM #2 Matenet connector…
Hi Avtar
The register programming that you pointed out the last post did not help to send the basic "ping" command between two DP83TC812 EVMs.
1. How do we set Master on EVM2 and Slave on EVM2 ?
I did follow the following.
But, programming…
Hello Faruk,
Can you share a block diagram for your current setup with EVM and PC. Our DP83TC812 EVM board doesn't have a processor on board and can't assign an IP address to it however you can assign a PC an ip address then connect it to our EVM's RJ45…
Hi David,
I had a call with customer today and let me update the status. Regarding test mode 5 issue customer will test the scrip that you suggest next week when their own PCB back next week.
At this monent, they would like to try connect DP83TC813EVM…
Part Number: TDA4AEN-Q1 Tool/software: Dear expert
SDK:ti-processor-sdk-linux-adas-j722s-evm-09_02_00_05
HW: TDA4entry
how to configure tda4entry SGMII and Serdes device trees? The driver for PHY Dp83TC812 was found on the TI website, and I don't know…
Part Number: AWR2944EVM Other Parts Discussed in Thread: AWR2944
Tool/software:
Hi,
In the demo High end corner radar demo, in the AWR2944 EVM ,only DP83tc812 works. There are two PHY addresses as belows:
in the ti_board_config.c file:
static const EnetBoard_PortCfg…
Part Number: DAC3482 Other Parts Discussed in Thread: DAC3484 Tool/software: Hi Team,
For evaluating the DAC3482 I am using the EVM but its has only single ended output,
Is it possible to work in diff mode?
1. Please advise how to install the "DNI" resistors…
Part Number: DP83TC812S-Q1
Tool/software:
HI,
PHY can Link UP,PHY can output 25MHz clk. but it cannot ping.
Is it possible to loop back?
How can I confirm that MAC to PHY can communicate?
The PHY driver is downloaded from here.
www.ti.com/.../DP83TC812S…
Part Number: TDA4VH-Q1
Tool/software:
Hi,
we are facing some problems with the integration of the TDA4 DSS & the UB941 Serializer. Following the bring-up guide we are currently stuck here:
What we tested already:
The DSI output works with the DSI…
Part Number: DP83TC812R-Q1 Hi Ethernet team,
My customer use DP83TC812 and they find that there is sawtooth wave at DP83TC812 physical layer (DP/DN) in PMA mode1. Do you have ever meet this issue?
1. Could you please help to analyze the reason?
2.Please…