Part Number: DP83TG720S-Q1 Other Parts Discussed in Thread: DP83TC811R-Q1 ,
Hi,
I have some DP83TG720S-Q1 EVM.
I notice that "temperature_output_code" is different value in each EVM under the same conditions.
Is this "errata" or "specification…
Hi Xiaofu,
If you are referring to the configuration script used for the DP83TG720 EVM, then it is under NDA and cannot be shared on a public forum like E2E. If you would like the script and have an NDA, contact your FAE to reach out to me through email…
Hi Adrian,
I have some DP83TG720S-Q1 EVM.
I notice that "temperature_output_code" is different value in each EVM under the same conditions.
Is this "errata" or "specification" ?
Regards,
Sambon
Hi Asha,
here is 32 bit log result root@j721s2-evm:/opt/edgeai-tidl-tools_09_02_09/edgeai-tidl-tools/examples/osrt_python/ort# ../../../../../vx_app_arm_remote_log.out & python3 onnxrt_ep_add.py
[1] 1314
[MCU2_0] 4.278639 s: CIO: Init ... Done…
The App is not working on any other core except C7x_1 for TIDL Node, below are the error logs we received during run stage, for these I ran the app with specific single core(C7x_2/3/4), also I ran the app with C7x_1 and it worked fine:
Error_c7x_2…
Part Number: TDA4VH-Q1 Tool/software: HI:
we now use the ethernat native driver base on SDK9.1 , but counter some problem:
- config Serdes1 LN2 and LN3 for SGMII-1 and SGMII2 ,Serdes2 LN0 for SGMII5 , now linux can detect phy and linked normal, but ping…
Hi Misa,
You are right. nova-slot5 is my J7 board.
I set up the DHCP server in my Ubuntu Laptop and trying to connect it to J7 but still "eth0" is not connecting to DHCP server.
When I type "dhclient -v" or "udhcpc -i eth0" on J7 board, it is…
Hello,
The EVM provides the mode selection for for the convenience of customers' evaluation. You can also reserve the selection on your board. The PWM frequency can be selected on AM0~AM2 pins, please find detailed explanation in section 7.3.16 in the…
Asha,
Regarding Bug PDK-7605 and recommendation of stack sizes being 32KB, I appreciate your confirmation that this issue is NOT a SYSBIOS specific issue but rather a fundamental C7x architecture issue meaning it's an issue regardless of the OS being…