Part Number: DP83TG721S-Q1 Hi, I refered following URL to confirm device driver for DP83TG721S. www.ti.com/.../ETHERNET-SW However, it seems that you prepare only for DP83TG720. Can we get device driver (Linux/RTOS either is fine) for DP83TG721S ? Best…
Part Number: DP83TG721S-Q1 Hi TI members,
I have an EMAC/PHY Suspend → Resume KPI issue.
DP83TG720_reset() is called three times during DP83TG720_chip_init() . Since DP83TG720_reset() contains a fixed 100 ms delay , it adds at least 300 ms to the…
Part Number: DP83TG721S-Q1 Hi TI Team, Please find the schematic of Ethernet DP83TG721S-Q1 for review, Kindly share your valuable feedback on the same.
The design Considerations are,
Interface: SGMII
Application: 1000BASE-T1 to Automotive Connector…
Part Number: DP83TG721S-Q1 Other Parts Discussed in Thread: DP83TG720S-Q1 , Hi, My project is using DP83TG721S-Q1, but I couldn't find DP83TG721S-Q1: Configuring for Open Alliance Specification Compliance (Rev. B) online. I could only find DP83TG720S…
Part Number: DP83TG721S-Q1 Hi team,
may I ask for answer in regards to pending questions:
1) Why is 100MHz the decisive frequency for the Ethernet transceiver DP83TG721S Q1? It is the 4th overtone of the quartz frequency. Why is the fundamental frequency…
Part Number: DP83TG721S-Q1 Hi team,
In the data sheet of the DP83TG721S Q1, different ferrite beads are recommended for the three supply rails VDDIO, VDDA and VDD1P1. Q uestions: 1.Can you please explain what criteria are used to select these ferrite…
Part Number: DP83TG721S-Q1
The design checklist recommends an 0805 package for the CM termination. I would like to understand wheather this package specification is hard requirement or if it can be replaced with an 0402 package of the same value
Part Number: DP83TG721S-Q1 Other Parts Discussed in Thread: DP83TG721EVM-MC Please suggest if there is any Eval Board for the above part number. We would prefer to test the 1000Base-T1 Interface before we put into Production.
Part Number: DP83TG721S-Q1 Tool/software: Hi Sir
When we use SOC(ex. RK3562) connection to DP83TG721S-Q1 for AVB function, than we need additional drivers or software to implement the IEEE 802.1AS、IEEE 1588v2、IEEE 1722、... protocol? If need , the will…
Part Number: DP83TG721S-Q1 There are multiple Vdd pins for the IC DP83TG721SRHARQ1. Requestign you to provide details for current consumption as well for the pins. Maximum supply current for each VDD pin , quiscent current as well.