Part Number: DRV2700EVM-HV500 I'm running windows 10 and trying to connect to my DRV2700EVM-HV500 but the device is not recognized by piezo control console. When I try to follow the firmware update/scan device procedure the board doesn't show up, I just…
Part Number: DRV2700EVM-HV500 Other Parts Discussed in Thread: LDC2114EVM , , LDCTOUCHCOMCOILEVM , DRV2700 Hello,
I would like to ask some questions regarding trigger operation. DRV2700EVM-HV500 can be used in trigger mode. What kind of signal is needed…
Part Number: DRV2700 Other Parts Discussed in Thread: DRV8662 , , Hello,
I could not find any information related to safety and isolation of the DRV2700 chip or its equivalent the DRV8662. We have been working so far with the DRV2700EVM-HV500 modified…
Part Number: DRV2700EVM-HV500 Other Parts Discussed in Thread: DRV2700 , LDC2114 , LDC3114 , MSP430F5510 Hello,
I am making a trackpad demo using DRV2700EVM-HV500. In order to make it, the firmware needs to be modified. However, I am not familiar with…
Part Number: DRV2700EVM-HV500 Other Parts Discussed in Thread: DRV2700 , , DRV2700EVM , DRV8662 Dear Sir/Madam
I would like to have a positive and negative high voltage driver for the piezo pump do you have any suggestions can I use DRV2700 another…
Other Parts Discussed in Thread: DRV2700EVM , DRV2700EVM-HV500 , DRV2700 We did test your DRV2700EVM-HV500 and DRV2700EVM with our EAP type haptic actuator, with capacitance over 200nF and which should be driven at 212 Vpp (0 – 212V) with frequencies…
Part Number: DRV2700EVM-HV500 Other Parts Discussed in Thread: LDC3114 , DRV2700EVM
Hi,
DRV2700EVM-HV500(EVM) has a trigger button for operation without using GUI. In order to use a trigger button, the MSP needs to be programmed. Could you write a…
Part Number: DRV2700EVM-HV500 My customer is using DRV2700EVM-HV500 to output 24V DC, his Piezo module need 24V DC. So how to do the modification on the board, is there any way he can add his R and C to drive the output to 24VDC?
Part Number: DRV2700EVM-HV500 Hello,
I set the waveform as the picture billow using Piezo Control Console . I want this waveform to be output only once when I click "Send Waveform". But the waveform was output 4 times. What caused this to happen?
…
Part Number: DRV2700EVM-HV500 Dear Sir/Madam
I hope you are doing well.
I am using DRV2700-HV2700 for driving a piezoelectric pump and I have two problems while connecting the EVM to the computer via USB the output is higher than the voltage selected…