Other Parts Discussed in Thread: DRV421 , DRV411 , DRV425 Hello,
We have requirement for 1600V high voltage sensing and 360A current sensing (low side shunt 50uohm).
voltage accuracy - =/-10V
Current sense accuracy = 1% FSR
Kindly suggest the…
Part Number: DRV425EVM Other Parts Discussed in Thread: DRV425 Hi Team,
A customer needed help in bus bar calculation. The application has a 15mm thick bus bar and the calculator available on our site only goes up to 12.7mm
The "Bus bar" and "3…
Part Number: DRV425EVM Other Parts Discussed in Thread: DRV425 Hi Team,
Can you please help us regarding the customer's concern below.
I have been experimenting with the DRV425 and I am consistently getting an output value that is 1.31 times the value…
Other Parts Discussed in Thread: DRV425 Hi Team,
Our customer is looking for a current sense IC that can measure up to 300A with an operating voltage of 3V to 5.5V. I used the Power Monitor Calculator to find a suitable device but it seems the recommended…
The specific DRV425 specifications are in the DRV425 datasheet. Below are the specifications for Vref for convince, but please view the datasheet of the DRV425 for further information.
The ADC you mentioned you can make differential measurements. You…
Part Number: TMCS1100 Other Parts Discussed in Thread: AMC1300 , DRV425 Measuring +-300amp current from a welding machine, can TMCS1100 be used in parallel to meet this range?
Part Number: DRV401 Other Parts Discussed in Thread: DRV425 Hi Team,
The customer wants to make a small size current sensor that can measure AC and DC to replace the current transformer. What is the accuracy of DRV401 and DRV425 in the full range of…
Part Number: DRV425EVM Other Parts Discussed in Thread: DRV425 We are evaluating the DRV425 fluxgate IC using the DRV425EVM evaluation module, and are seeing a substantial amount of ringing on VOUT. Please see the attached (YELLOW is Vout, Blue is Vref…
Part Number: DRV425EVM Other Parts Discussed in Thread: DRV425 , TIDA-00463 I am researching methods for building a magnetometer for conducting geophysical surveys to detect buried ferrous objects such as pipes or cultural items such as iron tools. These…
Part Number: TMCS1100-Q1 Other Parts Discussed in Thread: TMCS1100 , DRV425 Hi team,
My customer wants to use TMCS1100 in their BMS application but their current is 800A max, they are asking if they can connect multiple sense resistors in parallel…