Part Number: DRV603 Other Parts Discussed in Thread: DRV135 The output interface of the GLB circuit uses the RJ45 connector. During hot-plugging, there is a risk of damaging the DRV603. We would appreciate it if you could help identify the reasons and…
Part Number: DRV603 Other Parts Discussed in Thread: DRV602 , Tool/software: Hi,
I am considering replacing DRV602 with DRV603.
Q1. Is it possible to replace DRV602 with DRV603 with pin compatibility? Looking at the datasheet, it seems that the only…
Part Number: DRV603
Hi Team,
customer would like to design DRV603 in TV to driver line out or headphone out.
Would you please review schematic/questions and provide your comment?
(1)can DRV603 support headphone output 5mW with Load 32Ω?
(2)…
Hi, Alula,
Unfortunately, the DRV603 and similar products were developed as line drivers. The minimum load impedance that they support is 600ohms. So, this application cannot be handled.
Have you taken a look at our headphone amplifier product folder…
Hi Hugo,
Have you tried these 10pcs and NG part with the same external circuitry? I mean R26, R27 and R28 are the same for all tested parts?
I would like to confirm if the difference in voltage at pin 11 is related to DRV603 part or it could be related…
Part Number: DRV603 Hi all Would you mind if we ask DRV603PW? The customer consider using this device with Figure 13 configuration.(as second differential amplifier) DRV inputs connect to DAC output. DAC's offset is 2.5V. <Question> The customer would…