Part Number: DRV8436E Hi,
We got questions from our customers and would appreciate it if you could answer them.
The data sheet shows the min / max values for ΔItrip over the entire temperature range.
1. Is this "prone to max value in a high temperature…
Part Number: DRV8436E Hello guys,
One of my customers is considering replacing DRV8881E they using with DRV8436E for driving a step motor with lower voltage.
So they have a few questions as the follows. Could you please give me your reply?
Q1. When…
Part Number: DRV8436E Hi,
Could you please tell me latest mass production date of DRV8436E?
And will the DRV8436E be release in both 24-pin and 28-pin HTSSOP packages?
If both package will be release, is there any functional difference between the…
Part Number: DRV8436E Hi,
Can DRV8436E/P driver be used in new design? When will it be released for production? What case will be first released, PWP or RGE?
We recently acquired evaluation board DRV8436EEVM which includes DRV8436E driver in a HTSSOP…
Part Number: DRV8870 Other Parts Discussed in Thread: DRV8424E , DRV8828 , DRV8829 , DRV8436E Tool/software: Hello,
We using DRV8870 driver web tensioning application.
In this application we we driving motor in reverse direction and externally it…
Part Number: DRV8256PEVM Other Parts Discussed in Thread: DRV8436 , , DRV8436E DRV8256PEVM board is mounted a wrong IC DRV8436.
Meanwhile, this DRV8436 is P3DRV8436, not DRV8436P. DRV8436E could not match DRV8256P pin definition.
So, this DRV8256PEVM…
Marcos,
PHASE/EN interface device and PWM interface device are different device.
PHASE/EN interface device is named DRV8436E for a stepper motor.
PWM interface device is named DRV8436P.
The device, GUI interface and user's guide are different…
Other Parts Discussed in Thread: DRV8436E , INA186 , INA240 Hi Amp team,
In case of customer want to monitor the motor current by MCU,
We are recommending sense resistor in series with the motor coil winding between H-bridge as current monitor solution…
Hi Artsiom,
It may be possible to control solenoids with the DRV8889, but there are device that may work better.
Using a DRV8889 to control solenoids means the STEP/DIR pin need to be used to control the solenoids. It may not be possible to control…
Part Number: DRV8436E
I'm a little confused on the DRV8436P data sheet.
Assume for the moment we have the xDECAY input driven low (smart tune enabled).
I'm assuming for DRV8436E that, at all times, smart tune chooses the optimal decay mode based…