Part Number: DS100KR401 Other Parts Discussed in Thread: DS100KR800 , DS125BR401 Looking at the register set, each channel has (3) status or observation bits, but I can’t find a description of these bits. Can you please provide an explanation of these…
Part Number: DS100KR401 Other Parts Discussed in Thread: DS100BR111 , HI!
I need to add a re-driver supporting both 10G Ethernet and 1000-Base-X interfaces. Kindly clarify whether the below devices can be used for my application.
1.DS100KR401SQE/NOPB…
Part Number: DS100KR401 Hello!
I’m working with the repeater DS100KR401 Ultra Low Power and figured out some issues. In my project repeater is connected with FPGA Kintex-7, and I sent data from FPGA to reaper via I2C Interface (I’m using MicroBlaze…
Part Number: DS100KR401 Hello E2E,
Our customer is using DS100KR401SQE/NOPB with SFP+ Transceiver in 10.3Gbps application. They also want a Repeater bypass option, do we have an option available to bypass the repeater, or what is needed to do to bypass…
Part Number: DS100KR401 There are two different part numbers for the DS100KR401. One is DS100KR401SQE/NOPB and the other is DS100KR401SQ/NOPB. The datasheet does not detail what the differences between the two part numbers. Can someone explain the difference…
Part Number: DS100KR401 Other Parts Discussed in Thread: DPS-DONGLE-EVM
Hi team, Customer is designing the DS100KR401 application which used as the 10G Retimer. The DS100KR401 is configured as SMBus Slave Mode.
1. Is it necessary to configure or initialize…
Part Number: DS100KR401 customer would like do configurations setup to EEPROM file by sigcon tool.
the issue is that changing the setting in "low level page" but the setting does not able to mapping to EEPROM pages.
Can team teach how to do the setting…
Part Number: DS100KR401 Other Parts Discussed in Thread: DS125BR820 Hi Sir,
Does DS100KR401 be compliant for SFF-8431?
Do you have any test report of SFF-8431 compliance?
Please provide us the verification test report of this chip for our reference…
Part Number: DS100KR401 Other Parts Discussed in Thread: DS125BR820 , DS125BR401A , DS125BR401 I have a media converter design that converts between 10G-KR and 10G-SR (copper to fiber).
I was having issues getting the 10G-KR side to link/pass data.…
Part Number: DS100KR401 I am looking at the TI chip DS100KR401 and have a question about layout. Since these are 10G lines I would like to make them as neat and clean as possible. Shown below is the current layout that I have.....
My concern is…