Part Number: DS42BR400 Other Parts Discussed in Thread: DS25BR400 Tool/software: Hi E2E,
We are designing a screen display by using CML transceiver DS42BR400.
During the test, We found that the DS42BR400 surface temperature was to hot and the COF…
Part Number: DS42BR400 Tool/software: Hello, I'm in the process of choosing an Equaliser where I require x5 channels supporting a data rate up to 3.2Gbps. In my initial search this part appeared to be a potential contender, though the datasheet lacked…
Part Number: DS100BR410 Other Parts Discussed in Thread: EQ50F100 , DS38EP100 , DS25CP102Q-Q1 , DS42BR400 , , DS100BR210 , DS100DF410 Tool/software: Hi, In the response to DS100BR410: Thermal Characteristics - Interface forum - Interface - TI E2E support…
Part Number: SN65LVCP1414 Other Parts Discussed in Thread: EQ50F100 , DS38EP100 , DS42BR400 , , DS25CP102Q-Q1 Tool/software: Hello, I'm in the process of choosing an Equaliser where I require x5 channels supporting a data rate up to 3.2Gbps. In my initial…
Hi,
TI also has a large selection of repeaters that support up to ~3Gbps.
Another device you could consider would be the DS42BR400.
There are many parts available under the repeater/redriver section at www.ti.com/sigcon
Mike Wolfe
DPS APPS…
Hiroshi-San,
After running some test in DC couple mode using DS42BR400, our recommendation is to DC couple as long as the common mode voltage is about 1.3V. At other common mode voltages like 2V or 2.5V we recommend AC coupling since this is the most…
Hi Kajino-san,
The DS16EV5110 is specifically designed for a 3-data + 1-clock application. Four channel redrivers are common at datarates from 1.5 - 10+ Gbps. Here are some examples.
1.5 Gbps - DS15BR400
2.5 Gbps - DS25BR400
4.0 Gbps - DS42BR400…
Vidhya,
What is the problem with the single PowerGood output from the TPS65400? The TPS65400 is a good part for this design. Alternately, TI has a large selection of devices that can be implemented individually. You should follow-up on the power forum…