Hi Alex,
Did you try changing the dss configuration for "data-lines = <24>;" to "data-lines = <18>;"? Accordingly, adjust the hardware connection between the DS90C187 with AM5728. to ignore the two msbs for each R, G and B lanes.
Regards,
M…
Hi Casey,
That's an interesting idea. Do you know has anybody done this before for full-HD resolution at 60Hz?
Our full-HD dual-link LVDS display clock frequency is 73MHz, which in single pixel mode would mean 146MHz, still within TFP401A specs. …
Hello David,
The LVDS83B is not able to work with the requested resolution. You must to look at Texas Instruments WUXGA devices, like the DS90C187 or similar one.
Regards,
Gerardo
Hi Asaka-san,
Let's discuss this opportunity off-line. We have recently been seeing interest in automotive-qualification of the DS90C387, DS90C187, and DS90CF388A devices, so it would be great to understand the application, volume, and schedule for…
Hi Takishin-san,
By pull-down resistance value, I assume you are talking about the parallel data inputs?
I do not have a DS90C185 on hand at the moment, but I was able to probe the inputs of the DS90C187 on a C187EVK01. The pull-down resistance…
Hi,
Let me know if you have any questions.
Mike Wolfe \ DPS APPS
http://e2e.ti.com/cfs-file.ashx/__key/communityserver-discussions-components-files/138/1423.DS90C187-EVK.7z
Hi all,
I realize this thread started before the Ti acquisition of NSC was complete, so there weren't many dual LVDS options in the TI portfolio. However, Ti is able to offer a wider selection of LVDS output devices now that the acquisition has closed…