Hi Ohad,
Thank you for the schematic and the display picture.
Ohad Bonneh said: we have pulled up the clock legs to make sure that we are having perfect matching
What does this mean exactly?
Ohad Bonneh said: we still see 600ps jitter at the output…
Hi Tanveer,
In a DS90C383-DS90CF384 system, the clock can only be toggled from the transmitter (DS90C383) side. The DS90CF384 does not feature a strobe select toggle.
Since the system architecture above does not include a DS90C383 transmitter, the clock…
Part Number: DS90C383 Other Parts Discussed in Thread: , DS90CR285 , SN65LVDS93A DS90C383 has a status of NRND
But I did not find an alternative that would have a working temperature of -40°c to +85°c
How should I be?
Part Number: TFP401 Other Parts Discussed in Thread: DS90C383 We have built a customer HDMI board based on the TFP401 IC with LVDS out using the DS90C383 LVDS transmitter. We are connecting to a standard Windows 10 laptop for an HDMI source. On 6 bit…
The transmitter that goes with this device is DS90C383. This does not have the ability to alter any of the any parameters.
Usually these parameters are modified from the source before the serializer/deserializer.
Other Parts Discussed in Thread: DS92LV0411 , DS90C383 , DS92LV0412 , DS90CF384 , LV24EVK01 , DS92LV0421 I previously make a design using the DS92LV0411/412 IC to serialize 4 Ch+1Clk LVDS so that I can transmit it over fiber optic cable. My initial design was…
Other Parts Discussed in Thread: DS90C383 We are using Beaglebone with Angstrom 3.2.42 with LVDS LCD attached to DS90C383 LVDS transmitter. The display resolution is 1024 x 768.
When we run ts_calibrate to calibrate the touchscreen, if shifts the display…
Other Parts Discussed in Thread: DS90C383 , DS90CR287 Hello
Earlier, we used DS90S383MTD no problems. Subsequently, we replaced it of DS90SR287, circuit and elements unchanged. In most cases, the image on the LCD module is displayed without any problems…