Part Number: DS90UH926Q-Q1 [ DS90UH926-Q1 ] Color Pattern Discrepancy
Hi, Have anyone seen the behavior below? My customer now uses 0x64, Pattern Generator Control register, then see slightly different color on their screen.
One thing, I have notified is…
Part Number: DS90UH926Q-Q1 Dear Team,
As picture below:
When I write to SA ( VA(UH926)->SA(UH927) ), I hope the SA(UH927) will send a interrupt to SOC.
Do you have any suggestion?
I try to set the reg 0xc6 as 0x21 on UH927. But it doesn't work.…
Part Number: DS90UH926Q-Q1 I'm looking for an answer to the following question:
In case of an error in the BOM there are produced a lot of PCB with a Ratio at IDx Pin wich is not in the table:
Actual voltage is 2.5V instead of 2.399V. This is beyond…
Hi Hsu,
After device number 9xx, it is noted packing information. To check GPIO pin list, please refer to pin functions in datasheets ( DS90UB948-Q1 & DS90UB928Q-Q1 & DS90UH926Q-Q1 )
Best,
Josh
Other Parts Discussed in Thread: DS90UH925Q-Q1 , DS90UH926Q-Q1 Hello E2E members,
How do we calculation of latency between DS90UH925Q-Q1 and DS90UH926Q-Q1?
Assume a 720P video signal at 85MHz with 24-Bit color depth.
I saw a field that states 145T(DS90UH925Q…
Other Parts Discussed in Thread: DS90UH927Q-Q1 , DS90UH926Q-Q1 , DS90UH928Q-Q1 Hi i have an TFT LCD which is og 8-Bit (R0-R7,G0-G7 and B0-B7), i am using the DS90UH927Q-Q1
Can i use DS90UH926Q-Q1 deserializer to run my TFT LCD or do i need use DS90UH928Q-Q1…
Hi i have an TFT LCD which is of 8-Bit (R0-R7,G0-G7 and B0-B7), i am using the DS90UH927Q-Q1
Can i use DS90UH926Q-Q1 deserializer to run my TFT LCD or do i need use DS90UH928Q-Q1 along with the Driver IC which convertes FPD link III to RGB lines?
if need…
Part Number: DRA726 Other Parts Discussed in Thread: DS90UH925Q-Q1 , DS90UH926Q-Q1 , DS90UB949-Q1 , DS90UB948-Q1 As I am working on getting our analog camera working with the VIsion SDK I noticed that it has support for DS90UH925Q-Q1 and DS90UH926Q-Q1 Is there…
Philippe,
Thank you for your response.
Will the following FPD Link 3 SERDES combination work?
DS90UB947-Q1 --> DS90UH926Q-Q1 --> DLPC3438CZEZ
I understand the 926 will limit my max refresh rate due to 85MHz PCLK limit.
Thank you,
Tom