Hi Fajar,
Please define your expectations for higher performance.
There are other devices that use this simple serialization scheme for larger payloads, such as the DS92LV16 or the DS92LV18.
For higher data rates, the devices will typically employ…
Other Parts Discussed in Thread: DS92LV0422 , DS92LV2421 , DS25BR100 , DS25BR110 Hello,
We're using the DS92LV2421 serializer, DS25BR100 repeater buffer, DS25BR110 receive buffer, and DS92LV0422 deserializer. The components are located on three…
Other Parts Discussed in Thread: DS92LV2412 , DS92LV2411 , DS92LV2421 , DS92LV2422 Hello
I've downloaded the IBIS Models of the serializer DS92LV2411 and the deserializer DS92LV2412. We found out that the the serial input / output ports are not connected…
Other Parts Discussed in Thread: DS92LV2421 , TFP401A , TFP401 , DS92LV2422 Hello,
I am trying to serialize a standard 3-channel (plus 1 clock ch) TMDS signal (coming from a DVI - video only - source) down to one pair of wires. The total Bitrate should…
Greetings -
The DS92LV16 is an older generation Ser/Des and is in full production. The EVM (Eval Board) is no longer available.
The DS92LV18 is a similar part (18-bit) of the same vintage and a few boards are available for that device (see LVDS…
Other Parts Discussed in Thread: DS92LV2421 , DM3730 Hi
I'm working with AM/DM3730 on a CompuLab SOM, running Linux 3.0 and a camera connected to the parallel interface. Because the camera is 'far away' from the mainboard, the data is converted to a…
Other Parts Discussed in Thread: DS92LX1622 , DS92LX1621 , DS30BA101 , DS30EA101 , DS92LV0422 , DS92LV0421 , DS92LV2421 , DS90LV048A , SN75LVDS386 , DS92LV2422 , DS90CF383B Hi
I have to transmit a 14 bit differential data over about 60 feet at 50MHz…
Other Parts Discussed in Thread: DS92LV2422 , DS92LV2421 I need dc-balanced solution to ser/des random binary data of 18 bits at 62.5MHz clock. Can I use the DS90UR905Q/906Q serdes pair with HS=VS=DE=0 and six unused data lines also grounded?
It wasn…
Hi John,
Power design issues could be an issue, but pattern dependant issues usually point to signal integrity problems on the parrallel bus for these parts.
Can you probe the input signals on the serializer? Please check that the signals do not…