Amy,
It seems as though something like the DSLVDS1048 would be better suited then. However, the datasheet doesn't mention much about what happens below 200mVpp other than an affect to skew. Please confirm this chip would be better suited or if you have…
Hello Chuanfu,
Please see Differential to LVCMOS devices with output disable below
DSLVDS1048
SN65LVDS349
SN65LVDS33
Devices with output disable feature mostly appears in 4-ch parts. For LVDS and LVPECL we generally don't offer 1 channel devices with…
Part Number: DSLVDS1047 Other Parts Discussed in Thread: ADS7038 , DSLVDS1048 Hi Team,
our customer wants to use the DSLVDS1047 / DSLVDS1048 in a very time critical control loop with our ADS7038.
In order to be 100% sure that we do not have timing issues…
-Q1 devices might have a wider temperature range (not for the TXU0304), but the main difference is testing.
Regarding noise, the clock line would be the most sensitive one.
The cheapest four-channel LVDS devices are the DSLVDS1047/DSLVDS1048.
Other Parts Discussed in Thread: DSLVDS1048 , TMUX6112 Hello
I am using TMUX 6112 to implement an analog gate in combination with DSLVDS1048. But my output looks problematic. At the time of swiching, spikes are observed. The yellow waveform is the input…
Thanks a lot Emrys. I was thinking of doing things in an unnecessarily difficult way. I will apply this in my design. Btw, can I apply the same technique to reduce the Bandwidth of an LVDS signal (250MHz) to match with a LVDS TTL receiver( DSLVDS1048…
Part Number: DS90LV048A Other Parts Discussed in Thread: DSLVDS1047 , SN65LVDS047 , DS90LV047A , DSLVDS1048 Hi team,
Could you give me comment on following customer questions?
Q1. Can DS90LV048A be worked with SN65LVDS047 or DSLVDS1047 instead of DS90LV047A…
Hi Patrick,
My apologizes for the delay. Unfortunately we do not have a 8 channel receiver with active fail safe. There are only 4 channel alternatives like SN65LVDS32B or DSLVDS1048.
Hi Avi,
Please take a look at DSLVDS1048. This the receiver side.
http://www.ti.com/lit/ds/symlink/dslvds1048.pdf
Please note rise/fall time worst case is 1nS with CL of 15pF. I am not able to find a part to meet max 0.7ns with CL of >45pF.
Regards…