Other Parts Discussed in Thread: DUAL-DIYAMP-EVM Does TI provide the board design files for these development kits? Having this data would help create a solder paste mask.
Other Parts Discussed in Thread: DUAL-DIYAMP-EVM Does TI provide the board design files for these development board kits? Having this data would be useful for creating a solder paste mask.
Hello Luis,
Thank you for ADC reference circuit and simulation results.
Do I need R3 4.02ohm and R4 200mohm for real circuit, or are they used for simulation.
Please tell me what is the required tolerance for resistors around THP210.
I will create test…
Part Number: UCC14240-Q1 Other Parts Discussed in Thread: UCC5871-Q1 Hi,
Q#1:
I'm trying to match the UCC14240-Q1 DESIGN CALCULATOR TOOL calculations (dual output) with the existing UCC14240 EVM components.
In the spreadsheet, for IQ_DRIVER_VDD & IQ_DRIVER_VEE…
Part Number: DIYAMP-EVM Hi Team,
The gain of the evaluation board is determined by the resistor R1 and R2. Is the gain adjustable? When I bought this evaluation board, were R1 and R2 soldered, or were they adjustable resistors? I didn't find the values…
Hey Roger,
This app note covers how we modernly test our op amps: EMI Rejection Ratio of Operational Amplifiers (With OPA333 and OPA333-Q1 as an Example)
Figure 10 shows the circuit configuration, the DIY amp boards can be used to build a buffer (gain…
Part Number: DLPC900
Hi Guys,
I'm posting this concern from our customer and we require your help to clarify things up.
question1:On the Dual DLPC900 EVM board, there are two DLPC900 controller chip, one is master function chip, another is slave…
Other Parts Discussed in Thread: DUAL-DIYAMP-EVM , OPA657 Hi
I would like to know what is the maximum design frequency DUAL-DIYAMP-EVM's PCB board can support up to. For example, if I want to use OPA657 (1.6GHz Opamp) to build an non-inverting amplifier…
Part Number: LM25149-Q1EVM-2100 Other Parts Discussed in Thread: LM25149-Q1 Hello Team,
Our customer want to evaluate dual phase operation by using 2pcs of LM25149-Q1 EVM but somehow they can't work well.
Can you please let me know the setup to perform…
Part Number: TAS2563 I have a TAS2563 stereo (dual mono) EVM powered by a lab supply 5V/6.4A to VBAT. I have been able to characterize the speakers. Works well with a single channel. The issue when I try to run a demo using two channels.
The setup is…