Your link is interesting but I do not think that it applies.
Here are the sysctrl.c and sysctrl.h from TivaWare 2.1.0.12573
I simply went to the OS directory and searched it directly.
//**********************************************************…
I think so ,but I don't find the reason after I checked distortion table ('237-1.txt') and code parameters.The mesh table generated is 'mesh0803.txt'.
Fullscreen
237-1.txt
Download
0.1 0.00527
0.2 0.010539
0.3 0.015809
0.4 0.021078…
You can solder the TPS65941111 devices you intend to change onto the boards that will use them as '1213s by themselves. Then follow the instructions below before populating an '1111 in the PMIC-B location.
Hardware Setup
Solder target TPS65941111…
We're not sure what you mean by "shared transport driver". We're using
Debian's stable kernel for Stretch, plus a patch to add our DTS file.
Attached are the current kernel config and our DTS file (file extensions changed to accommodate filter) Below…
Other Parts Discussed in Thread: CONTROLSUITE , DRV8305 Hello,
I'm working with this example from ControlSuite, and passing Level 2 Incremental Build i have to see some waveform of clark1.Alpha, clark1.As and currents.
Instead of seeing sinus i see…
Older revisions of the manuals are not generally available for public download. Most of the time, using the latest manual is good enough. All that said, I can understand why you might want an older manual.
This one ...
Peter Adamus said: the "ARM…