Hi Kevin,
I assume SmartRF Flash Programmer 2 uses the serial to identify the device, and probably falls back to the CC2642R when it cannot be identified. As of why you are seeing multiple devices, I'd believe this is due to the fact that SmartRF Flash…
Part Number: MSP430F67691 Other Parts Discussed in Thread: MSP-FET , UNIFLASH Tool/software: I'm currently experiencing problem with flashing the MSP430F67691 controller via the MSP-FET emulation tool in Spy-Bi-Wire mode.
software used: FET-Pro430 …
Hi Arthur,
We use Flash Programmer 2 for Production so would be a big change to move to UniFlash for this little reason. Could you please check if it works with Flash Programmer 2 at your end? It surely works when using Flash Programmer 2 GUI.
…
Part Number: CC1310 Other Parts Discussed in Thread: UNIFLASH Hello, I'm developing a Python scrip to automate flashing firmware. I want to control Flash Programmer 2 using CLI but I cannot connect to a device. I list connected devices using the command…
Hi Siri,
Thank you for the support.
Siri said: Are you talking about the SmartRF Flash Programmer or SmartRF Flash Programmer 2?
Which revision are you using?
SmartRF Flash Programmer 2 ver1.8.2 is being used which worked before.
Siri said:…
Part Number: CC1352P7 Other Parts Discussed in Thread: CC1352R , UNIFLASH Hi all,
I have a board with CC1352P7. I need a way to read and write specific memory locations via a tool.
I usually use Flash Programmer 2 for CC1352R:
But apparently…
Part Number: TMS320F28379D Tool/software: Hello There,
I am currently working on serial flash programming with TMS320F28379D. I've looked at this document and configured GPIO72 -> 0 and GPIO84 -> 1 . I configured SCI boot mode with this configuration…
Part Number: TM4C1290NCPDT All,
we're using LM Flash Programmer to upgrade FW and sometimes noticing, in an unpredictable manner and only on some PCs, the following:
Sometimes no communication via USB
In other cases the procedure doesn’t get to…
Part Number: LAUNCHXL-F28069M Other Parts Discussed in Thread: C2000WARE Tool/software: Hello,
I try to reprogram F28069M Launch board using SCI.
I place IO in correct sequence. I used CodeSkin software and serial works, reprogramming too (with C2prog…
Part Number: CC2642R Hello,
I have a weird bug occurring with a CC2642 board where it will not let me program it directly through Code Composer Studio, however it does let me program it through Flash Programmer v2.
However, since I my program is using…