Hi Sreenivasa,
1. Yes, customer wants to measure MSE by fixing the voltage on the master and slave. Customer succeeded to do MSE measurement with auto-nego mode and failed to do it with Forced mode. So the original question from customer is, why he…
Hi Gerd,
I discussed this issue with some of the C2000 experts. They were able to point me to the correct document for C2000:
/cfs-file/__key/communityserver-discussions-components-files/171/SPRU151A.pdf
However your issue of why you are unable…
Sri,
The customer has come back with the following comments:
However the answer is very confused.
Please see attached TI schematic of the evolution board of ONET1151L. As you can see, the data input, TDP and TDN, directly from PIN18/PIN19 of SFP…
Hello,
The GC6016 is not yet a released product. When it is released, the released datasheet will be available on the GC6016 portion of the TI webpage.
A preliminary datasheet is attached (this is not the final version, final specifications are…
Part Number: J6EVM5777
I am working with a EVM5777BG-03-00-00 board and trying to use the pre-built Android Oreo binaries from here .
I have followed the release notes, to flash the eMMC with the oreo system images.
However the the system services…
Part Number: J6EVM5777 Other Parts Discussed in Thread: DRA742 , PMP , DRA752 , TVP5158 , CSD
Hi,
I am trying to boot J6EVM5777 with Android Oreo following the instructions in the Release notes using pre-built binaries
However the Services keep…
Part Number: PROCESSOR-SDK-AM62X
Hi,
We developed an app and run on the am62x evm.
I found a problem that there is almost 1 second delay when switch activity(Image).
And the system log always display below log when the activity switched.
How…
Hi Hong, Here is SDK8.4 full log. Below line seems the error happens. [ 2.084076] mmc0: mmc_select_hs200 failed, error -110 SDK84_log.txt The customer does not keep SDK8.6 log, but the similar error was observed. Thanks and regards, Koichiro Tashiro
Hi,
Attached are the Boosterpack Pinout and MSP430F5529LP User guide. Please see Figures 40 & 41 in User Guide for Launchpad Pinouts. The unused lines (GPIOs) on the P2 & P3 of the BOOSTXL-CC1120-90 can be used for your Keypad.
If you change the Pins…
Part Number: DRA745 Tool/software: Linux Hi Team,
we use Soc DRA745, 4G RAM, software build and download reference by http://omappedia.org/wiki/6AM.1.3_Release_Notes .
issue: out of memory. oom-killer was triggered, kill process again and agina till…