Part Number: TDA4AH-Q1 Tool/software: Hello,
Our design includes the TDA4AH and a Micron MT53E512M32D1 LPDDR4 IC. While running compliance testing I am encountering very slow slew rates that do not meet the JEDEC LPDDR4 specifications. We are running…
Part Number: SK-AM62
Hi TI Team
Is supported OTA update on Android 14?
I built Android and the OTA packages for SK-AM62 and then i updated the eMMC using update_engine_client.
- built Android images: m TARGET_AVB_ENABLE=true
- built OTA packages…
Hi Dave,
It's not so uncommon to see different programmatic behavior when JTAG is removed from the debug simpulator, executes code much slower than in real time CPU speed. What you are describing sounds like one or several subroutines are executing…
I add a bbappend for tisdk-base-image, I add some new package, such as inxi fio glmark2 sysbench coremark stress-ng.
I get error when adding these package, if I remove there's no error.
I can attach a whole log for this issue. DEBUG: Executing python…
Part Number: TMS320F28375D Hi, team,
Could you please give me your advice how to connect Encoder?
When user connect F28375D to R/D converter with serial communication as Page 40 of attached file, should user use SPI peripheral in F28375D?
MNL000634W00_AU6805_20161214…
Hi,
So perhaps I will share more of the settings of the Tektronix setup.
Basically I was following to Tektronix 1000BASE-T1 conformance test suite.
I am using a Tektronix scope MSO64 with the 1000BASE-T1 Automotive Ethernet PMA test suite.
I attach…
Hi Venkat,
1. I use /dev/fb0 to do RGB888 output test.
2. I now turn OFF "FB_OMAP2" and turn ON "OMAP DRM" in menuconfig, "CRTC" set to 2. I also add "drm.debug=0xff"
Fullscreen
7608.boot log.txt
Download
U-Boot SPL 2016.05 (Apr…
Hi dev123 - Omer,
There is some oddness around arrays and longs. The C2000 compiler guide Optimizing-C gives clues, by default bytes are 16 bit and seemingly w0_w1[2] is actually 32 bit long. Oddly longs do not behave well in C lib arrays data often…
Hello Sahin,
I developing on the ARM side and I running SYS/BIOS 6.73.00.12. I developing my project on the inherited code which was initially developed using StarterWare. I have problem with MMU because when I try to run this an exception occurs. Therefore…
slas667b.pdf Hi,
Thanks for the reply.
Here there is confusion with i2c device address.
As per attached datasheet of tlv320aic3100 , on page no:20 I2C device adress is 0x18 ,and on page no 78 it displayed as 0x30.
so whats the i2c device address…