Hi Krunal,
Here is more debugging info.
root@am335x-evm:~# dmesg |grep -i pvr [ 15.291247] [drm] Initialized pvr 1.17.4948957 20110701 for 56000000.gpu on minor 1 [ 30.351649] PVR_K: UM DDK-(4948957) and KM DDK-(4948957) match. [ OK ] root@am335x…
Hi Krunal,
thanks for the reply.
> Yes, we are experiencing a similar issue with Qt but our colours are not inverted. ... we are not able to launch a Qt application with the eglfs flag ...
Thanks for the update. Just to be sure we are experimenting…
Hi Aaron, sorry for my late response, but I got sick last week. Currently we have 3 Test-Setups: Topology of Setup 1: Topology of Setup 2 and 3:
The difference between 2 and 3 is that there are different modules attached to the EtherCAT SubDevices…
Hi,
It may not need to run in FDU mode. You can add MSPM0_BSL_GUI.exe in SDK installation folder\tools\bsl\BSL_GUI_EXE. Modify the attach file name from .txt to .exe
MSPM0_BSL_GUI.txt
Then run the .exe file. In MoreOption->Update XDS110 firmware…
Part Number: TDA4VM
Tool/software:
Hello,
We are trying to run out model on EdgeAI 9.20.07 . https://github.com/TexasInstruments/edgeai-tidl-tools/tree/09_02_07_00?tab=readme-ov-file .
We have observed issue with Matmul layer on target when…
I have followed the steps suggested and i am still facing the same issues with the input , i have added all the plots here for more analysis
comparision_outs.zip.txt
Fullscreen
tidl_importfp32.txt
Download
modelType = 2
numParamBits…
1. The booting of u-boot fails in the SPL before any console output. Is there something else I could provide that would help? 2. The same emif registers values are used for both emif1 and emif2. See attached *.xlsm file for calculation of emif values…