Part Number: DIFFAMP-EVM Other Parts Discussed in Thread: OPA207 I'm trying to utilize the DIFFAMP-EVM to output the difference between two signals at approximately 2.3V. When I attach those two signals to VIN+ and VIN-, I see an output around 1.15V.…
Part Number: INA105 Other Parts Discussed in Thread: OPA180 , INA597 Hi Ti
Could you help to check the DMM design for us?
DMM SCH
1.Constant Current Power design:U22 INA105KU+ U26 OPA180ID
MCU control Switch and change output current,Could…
Part Number: INA105 Other Parts Discussed in Thread: INA133 , INA132 I am using the INA105 in a difference amp configuration to receive a signal output which can go up to +10.5V. When the input signal rises above +9V the output of the INA105 will follow…
Part Number: INA105 I have a question about cross reference solution:
This Analog PN “AMP03GS-REEL” has cross part INA105KU/2K5 with code (Q: Same Functionality & Pinout) and according to the description of Q type it is not exact equivalent , I compared…
Hi Tamara,
I have been doing some further testing and have been getting some results, which is a start!
My application is a CNC router build, that uses a desktop PC PSU which I'm piggy backing off the +12V and -12V outputs on the 24 Pin ATX connector…
Soenke
We haven't heard back from you so we assume this answered your question. If you need additional help just post another reply below.
Thanks
Dennis
Hi Alexander,
Can you please provide a schematic showing all of your connections and inputs to the INA105?
Thanks,
Zak Kaye
Precision Amplifiers Applications
Other Parts Discussed in Thread: INA105 , BUF634 Hello,
I'm trying to make a voltage-controlled current source to control a laser module (Flexpoint dot laser module 635nm, 4mW, DC 4.5-30V).
I want to provide a limited current (0-100mA) according to…
we are using INA 105 in one of our instrumentaion applications. The range of signal we intend to use is from 0mV to 30 mV. We are using in differential mode with Unity gain. The problem we are facing is the noise obtained is around 150mV. We have used…
Part Number: INA133 Other Parts Discussed in Thread: INA105 Tool/software: Dear , Instrumentation Amp Support team . We at Disty have issued PCN No. 20250326007.1 to our customer.
RFAB has been added, but our customers are concerned about the CMRR performance…