Other Parts Discussed in Thread: PGA2500 hi sir:
About PGA2500 , I have aquestion to ask.
It is that when I try to adjust PGA2500 level shift to support the AD input range 0~5.
But it is not work. I am not sure that I control is corrected or not.
Links are…
Other Parts Discussed in Thread: INA826 , INA118 , INA110 INA826 Datasheet Version SBOS562E –AUGUST 2011–REVISED APRIL 2013 have MAXIMUM Input voltage range as (–VS) – 40 to (+VS) + 40 V, and
max typical use of +/- 40V.
I'd like to…
Other Parts Discussed in Thread: INA121 , INA116 , PGA280 , INA111 , INA110 , TIPD135 , REF200 , TIPD101 , TIPD107 , ADS1248 , THS4521 Problem : 1. I have to make a null detector with MCU. 2. Input voltage maximum is 30V dc. 3. Current to detect is 1nA to 300mA. 4. Galvanometer…
Other Parts Discussed in Thread: INA110 Hello,
I have a resistive linear position transductor (potenciometer) whose position I need to read from a remote station. I design a system using a constant current source (2 wires) to produce a constant voltage…
Hi Peter,
thank you so much for your detailed reply. I appreciate it!
As you said, INA131 and INA110 seem to be very good candidates for me! I oversaw them when I was looking for sense amplifiers.
1) In your simulation, you used a ref voltage of 2…
Other Parts Discussed in Thread: INA118 , INA111 , INA110 , INA166 , INA163 , THS4221 , INA826 , INA331 , OPA365 I would like to use an instrumentation amplifier to amplify a strain gauge bridge signal (on the order of mV) to an amplitude of V (a gain of 1000…
Other Parts Discussed in Thread: INA110 , INA217 , INA128 I have a circuit that I originally put together a couple of years ago and it seemed to work quite well. It is an amplifier for a low impedance sensing element (around 25 ohm) that puts out a very…