Part Number: INA118 Tool/software: I am using INA118UB. The maxmium output was 2.6V, when the power supply is ±3.2 V. This is consistent with the parameters in the manual.
These parts maxmium output are 2.6V @ ±3.2 V power.
But when I bought…
Part Number: INA118 Other Parts Discussed in Thread: INA821 Tool/software: Hello E2E Experts,
Good day.
The instrumentation operation will be used to capture the ECG or EMG signal, these signals are very small and come in mV from the human body.
The instrumentation…
Part Number: INA118 Good morning,
I just wanted to check what is the platting of P/N INA118U or P/N INA118U/2K5.
In the datasheet, it states the following: Call TI | NIPDAU.
If we order one of these P/Ns, are we going to receive always NiPdAu?
I know that…
Part Number: INA118 Dear ladies and gentlemen,
We ordered the INA118P instrumentation amplifier from our distributor. After that we got the feedback that they want to deliver us the INA118PG4, because the INA118P is not available anymore. Is there a difference…
Part Number: INA118 Other Parts Discussed in Thread: INA188 , PGA308 , PGA309 Hi,
we are using the INA118 for amplification of a strain gauge force sensor. The unloaded sensor output voltage can vary between +64mV to -64mV due to tolerances of sensor and…
Part Number: INA118 Hello ...Are INA118U and INA118UB coming from the same die?
if yes then I can assume the wafer is screened and each element is sorted out for either INA118U or INA118UB
or if INA118U and INA118UB are not sharing same device then we…
Part Number: INA118 Per this E2E post here , the only difference between the INA118U and INA118UB is the box size. However, the specs are different in the electrical characteristics table. Can you confirm they're the same?
Part Number: INA118
In the past two years, components are very scarce, so we often can't get materials from TI's agent Arrow.
However, materials can be purchased from other channels, but they often paint labels. What's the reason?
For example…