Part Number: INA122 Good afternoon,
I was wondering if the INA122 would be suitable to read the battery voltage of a 12v lead acid battery. the battery is located 10 feet from my charging circuit and if i try to read the battery voltage at the circuit…
Part Number: INA122 hi,
The circuit adopts positive and negative 9V power supply. When the power supply has no obvious glitch, the chip works normally.
When the power supply has large glitches (peak-to-peak value is 720mV, glitch cycle is 16.6us), the…
Part Number: INA122 Hi,
what is the difference between the INA122UA and INA122UAG4? I couldn't find helpful information about that...
Thanks and best regards,
Daniel
Part Number: INA122 Other Parts Discussed in Thread: LOG114 , OPA388 , TINA-TI I am looking for a solution to measure the wide current range from 1uA to 300mA on a 3V rail . If it not possible to do for such high range and precision, we can further split…
Part Number: INA122 I have a customer asking if we any information on the common-mode input impedance for the INA122. He asked specifically for the input impedance to GND, but I believe that he is looking for the common-mode impedance for this part. Do…
Other Parts Discussed in Thread: INA122 Dear:
INA122 Question:
1.Circuit diagram is as follows,when S-=0V,S+=1V,G=7,VCC=22v,now and then the Vout=22V,
nomoral the Vout should 7V,why?
Other Parts Discussed in Thread: INA122
I have a problem using an instrumentation amplifier(INA122), www.ti.com/.../ina122.pdf I've used the scheme in page 9 figure 5. Is powered by +5volt from arduino diecimila. The bridge have 2 resistors of 10k ohm…
Other Parts Discussed in Thread: INA122 Hello,
Can I know the Application Circuit for the INA122 IC for the Pulse Oximetry Principle ?
Please reply on this ASAP.
Other Parts Discussed in Thread: INA122 , INA126 Hi, thanks in advance for your time and expertise.
I am using an INA122 to measure input and output voltage in an GaN inverter.
When I measure the sensor response with the scope when the circuit is not switching…