Part Number: INA168 Tool/software: I am using the INA168 in an application where the current swings from 0 to 3A. The INA168 is powered from a +5V supply. The common mode voltage is approximately +43V. I am using a 0.1ohm sense resistor and interested…
Part Number: INA168-Q1 Other Parts Discussed in Thread: INA168 Tool/software: Hello All,
I am using INA168QDBVRQ1 in my card.
RS=0.02 ohm
RL= 200kohm
CL=100p
I am measuring current on 24dc motor with PWM of 10khz 30%
the dc motor resistance…
Part Number: INA168 Dear team,
Please help provide the functional description and the recommended HS Code for INA168NA/3K.
Thanks.
Best Regards,
Laura.zhao
Part Number: INA168-Q1 Other Parts Discussed in Thread: INA168 , INA186 Hi All,
I am using the component INA168:
RS = 0.01 OHM
RL = 133KOHM with 100pF parallel capacitor
after it i have buffer amplifier AD8615 with RC output R=10ohm C=1nF and…
Part Number: INA168 Other Parts Discussed in Thread: OPA333 , INA138 Tool/software: Hi,
my customer asked about the power supply of INA168 (and OPA333) in app note SBOA198A :
Questions
Could you please give me a clear example of what a correct…
Part Number: OPA991 Other Parts Discussed in Thread: LM321 , TL071 , , INA168 , TLV9351 Tool/software: Hello,
We want to put out a 4-20mA current (process control) from a filtered PWM.
Since we set it from a micro, it is low-sede, but we need a high…
Part Number: INA168-Q1 Other Parts Discussed in Thread: INA168 , INA240 Tool/software: When FOLD operating,
I checked voltage between OS MRR shunt In and OS MRR shunt Out is 73 mV.
And Shunt Forward voltage 395 mV So we can calculated 732 mA.
And…
Part Number: INA168-Q1 Tool/software: hello everyone, In my application, the maximum current reached 40A, Assuming I set the bias voltage to 1.65V according to the diagram, can the chip output such a high voltage with VOUT=1.65V+40A * 200K * 2m/5K=4.85V…
Part Number: INA168 Good morning,
I have been looking at the datasheet for INA168NA and I don't know why the operation temperature is only defined for the P/N of the 3K reel (P/N INA168NA/3K) but not for the 250 un reel (P/N INA168NA/250)
I suppose…