Part Number: INA168 Hi Team,
I found INA168 and INA168-Q1 use same package but with different size, INA168 is much bigger than INA168-Q1, is that correct?
My customer want to find a device which is totally P2P with INA168-Q1, but non-automotive qualified…
Part Number: INA168-Q1 Hi team,
What's the Vsense input minimum voltage of INA168-Q1 with 100mohm Rs?
Because when my customer set load Is=10mA, means Vsense=Rs*Is=1mV only. In that case, the output voltage is not s expected. Can our device work properly…
Part Number: INA168-Q1 Other Parts Discussed in Thread: INA168 , INA219 , , INA226 This is in regards to the input filter of the INA168:
A 0.100 ohm current sense resistor is being used as Rshunt to measure a current 0 – 500 mA. They would like to use…
Other Parts Discussed in Thread: INA168-Q1 Hello, There are the typical and maximum total output error of INA168-Q1 at the condition of Ta=-40~125C. Can I use typical value as value at the condition of Ta=25C? Our customer will confrim the system specification…
Other Parts Discussed in Thread: INA281-Q1 , INA168-Q1 , INA138-Q1 There is no mention of any automotive qualification standard for INA170EA Current shunt in its datasheet, can we use it for automotive applications,
If not suggest us the alternate current…
There are two automotive 60 V current sensors with adjustable gain: www.ti.com/amplifier-circuit/current-sense/analog-output/products.html#p726max=60;120&p773=Adjustable&p1498=Automotive
The INA169-Q1 has a bandwidth of 440 kHz, the INA168-Q1, 800 kHz…
Hi,
It is not recommended to adjust the gain externally. Please consider reducing the shunt resistor value as Kai suggested. In addition, we have the following lower gain options:
LMP8278-Q1 gain of 14; INA138-Q1, INA168-Q1, INA139-Q1 and INA169-Q1…
Part Number: INA168 Other Parts Discussed in Thread: , INA240 Team,
My customer is interested in INA168 and wants to know if INA168-q1 is fully bipolar technology or if it includes CMOS technology?
Thank you.
-Needhu
Other Parts Discussed in Thread: INA168-Q1 , LMP8480 Hi Team,
Do we have a replacement for the MAX4080? I found the INA168-Q1, which is as close as I could find, but I was wondering if we have anything closer..
Thanks in advance!
Jared